Other Parts Discussed in Thread: HALCOGEN
Hello,
I'm having problems getting a very basic program to step through the debugger and hoping that somebody can point me in the right direction. I have designed a board and think I have it running, JTAG appears to work. I tried the same setup with the Hercules development board and that behaves the same way, so I don't think it is a hardware problem.
Basically when I try to start the debug session, I don't seem to be able to do anything except hit the red "Terminate" button, everything else is grayed out.
I have tried CCSv5 and CCSv6 with a XDS100v2 JTAG, both do the exact same thing. JTAG tests out fine using the "Test Connection" button, so I don't think it is the problem.
The program is very simple, just added some code to the default "Hello World" program (tried commenting out the cout statement too):
int main() {
cout << "!!!Hello World!!!" << endl; // prints !!!Hello World!!!
for(;;)
{
volatile int i, j, k, x;
for (i=0; i<1000000000; i++)
for (j=0; j<1000000000; j++)
for (k=0; k<1000000000; k++)
{
x++;
}
}
return 0;
}
Using the debug build configuration. Tried the C version, same thing.
All I see on the console is:
CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset
CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset
Build reports this:
**** Build of configuration Debug for project test ****
"C:\\ti\\ccsv6\\utils\\bin\\gmake" -k all
'Building target: test.out'
'Invoking: ARM Linker'
"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.4/bin/armcl" -mv4 --code_state=32 --abi=ti_arm9_abi -g --display_error_number --diag_warning=225 --diag_wrap=off -z -m"test.map" -i"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.4/lib" -i"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.4/include" --reread_libs --warn_sections --display_error_number --diag_wrap=off --xml_link_info="test_linkInfo.xml" --rom_model -o "test.out" "./hello.obj" -l"libc.a"
<Linking>
warning #10247-D: creating output section ".text" without a SECTIONS specification
warning #10247-D: creating output section ".const" without a SECTIONS specification
warning #10247-D: creating output section ".bss" without a SECTIONS specification
warning #10247-D: creating output section ".cinit" without a SECTIONS specification
warning #10247-D: creating output section ".sysmem" without a SECTIONS specification
warning #10210-D: creating ".stack" section with default size of 0x800; use the -stack option to change the default size
warning #10210-D: creating ".sysmem" section with default size of 0x800; use the -heap option to change the default size
'Finished building target: test.out'
' '
**** Build Finished ****
I'm probably missing something stupid, but I can't think of what that might be.
Any help on things to look into or test would be greatly appreciated
--Tom