Other Parts Discussed in Thread: HALCOGEN
It seems that the latest HALCoGen release 04.05 creates a link command file that isn't taking over the steps from the following WIKI instructions:

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jan,
There are two steps involved to get this implementation to HALCoGen
1) Changing HALCoGen linker file generation.
2) Removing the default Auto ECC Generation in CCS.
Unless both are changed by default user will have ECC error.
Also with HALCoGen we do not want to disturb the customers compatibility.
We are evaluating to change the default CCS option to uncheck Auto ECC generation and generate the recommended linker file , but no firm decision has been made yet.
Thanks for the update, Prathap.
It is understood that step 2 is a manual step to be done by the developer when setting up the CCS project.
I've reported step 1 because I saw a message earlier that the modification of the generated .cmd file is a temporary action that would be covered in the next HALCoGen release.
That's why I tested this out after the release 04.05. When I saw that it wasn't handled, I created this ticket to report.