Other Parts Discussed in Thread: RM48L952, HALCOGEN
Hi,
I'm working on the RM48L952 HDK board and trying to make a serial communication using RX and TX pins of the board expansion connector.
I can connect through the SCI/LIN port using the Mini USB connector and the example code "example_sci_uart_9600.c", but the communication is not happening through these pins.
The SCI module was configured in HALCoGen, also the SCI pins are multiplexed with N2HET1[06] and N2HET1[13] in PINMUX module.
I would appreciate it if you could help me.
With regards,
Fatemeh