Other Parts Discussed in Thread: HALCOGEN
Hello,
I have to say that these TI forums are most excellent! Response has been very quick and useful.
Ok, onto my question. I have a TMS570LS0432PZ that I have used all the GPIOA lines on and I need more. I had connected up some external parts to the N2HET pins (19, 22, 25, 26, 90, 97, 98, 11, 64) t. How do I control them? Halcogen seems to have HET1 controls, am I done for?
I also want to bit bang the SPI1, SPI2 and SPI3 lines for now, can I do that?
Example code would be most appreciated, but I can understand if there isn't anything available. General instructions would be fine, I'll muddle through them.
Thanks!
--Tom V.