I just bought RMS57Lx LaunchPad
When I try Project 0 . I get below error when I run debug.
Error connecting to the target: (Error -260 @ 0x0) An attempt to connect to the XDS110 failed. The cause may be one or more of: invalid firmware update, invalid XDS110 serial number, or faulty USB connection. The firmware and serial number may be updated using the xdsdfu utility found in the .../ccs_base/common/uscif/xds110 directory of your installation. View the ReadMe.txt file there for instructions. (Emulation package 6.0.14.0)
I am using CCS 6.1 . It updated.
Project build configuration:
Varient : RM57L8xx
connection : TI XDS110 USB Probe
Compiler version : TI v5.2.4
OS:
I am using Ubunut 14.
There are two device shown in /dev/ when I connect board
ttyACM0
ttyACM1
Board Led Status
LED 7 , LED6 : on
LED 3 : blinking
I have used Project0 holacogen files.
I appreciate you time and efforts