Other Parts Discussed in Thread: TM4C1294NCPDT
I am trying to design a custom board using the TM4C1294NCPDT Launchpad as reference and using TM4C1294 as my uC.
The application guide states that the uC+PHY should be > 1in away from the magnetics/transformer and the RJ45 connector should be <1in away from the magnetics/transformer.
The problem I am facing is that my custom board will be connecting to a backplane where the RJ45 connector should be. Will having a connector in the ethernet line be a fatal noise problem? This unit would be put in a server rack environment.
PHY <- 2inches -> connector to backplane <-2inches-> transformer <- 1inch -> RJ45
I have read on general forums that its better to put the transformer closer to the PHY (basically before the connector) and have the distance between the transformer and the RJ45 be longer because "that is the point of having a transformer." <-whatever that means.
Or does none of this matter as long as you have a GND plane under the PHY <-> transformer and an Earth GND plane under the transformer <-> RJ45.
Thanks,
Andrew
Application guide for reference (http://www.ti.com.cn/cn/lit/an/spma056/spma056.pdf )