Hi,
I am using Hercules development kit and i use lwip 1.4.1 library. This library includes a header file which has define LWIP_HTTPD_SUPPORT_ POST. I can active some functions with setting this define to 1. But when i set it to 1 and build my project, i have seen some errors on console. These errors are below,
#10010 errors encountered during linking "BuildTMS570.out" not built
#unresolved symbol httpd_post_begin, first referenced in lwip-1.4.1/apps/httpserver_raw/httpd.obj
#unresolved symbol httpd_post_finished, first referenced in lwip-1.4.1/apps/httpserver_raw/httpd.obj
#unresolved symbol httpd_post_receive_data, first referenced in lwip-1.4.1/apps/httpserver_raw/httpd.obj,
Can anyone help me?
Regards.