Other Parts Discussed in Thread: TMS570LC4357, HALCOGEN
I have been trying to get the eCAP modules up and running on the Hercules TMS570LC4357 Launchpad.The eCAP modules can be used for either PWM generation or as capture input. I was able to get eCAP2 and eCAP3 module up and running in capture mode. eCAP1 module is not accessible from any pin.
eCAP 4, eCAP 5, eCAP 6 modules are not working in the capture mode.
I have configured the eCAP modules 2-6 in PWM mode and was able to generate PWM using all of them. This means that the PINMUX is able to configure pins to the appropriate module. Could someone help me figure out what the problem might be?