Other Parts Discussed in Thread: TMS570LS0432, HALCOGEN
Hello,
I"m trying to set up a TMS570LS0432 with the N2HET block. I installed the HET IDE and noticed that the chip that I need is not listed. Am I missing something? Is there another chip that could stand in for the one I need?
Another question I have is that I want two outputs from this block:
1) N2HET[0] : 4 to 8MHz square wave, should be simple i would think.
2) N2HET[22] 8bit or higher resolution programmable PWM with a 10mSec period, I know this is really slow, perhaps too slow? If so, I think it can be a be higher, perhaps 1mSec period, but not any higher than that. This is for backlight LED control.
Let me know anyone can help with this.
Thank you.
--Tom V.