This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Re: TM4C Microcontrollers Forum: how do i count rising edges of a square wave through the capture compare pin0 of timer0

thank you. i got it.


Sent from Samsung Mobile


-------- Original message --------
Subject: TM4C Microcontrollers Forum: how do i count rising edges of a square wave through the capture compare pin0 of timer0
From: Amit Ashara <bounce-310847@mail.e2e.ti.com>
To: TM4C_forum@mail.e2e.ti.com
CC:


 

A Message from the TI E2E™ Community
Texas Instruments

 

Amit Ashara replied to how do i count rising edges of a square wave through the capture compare pin0 of timer0.

Hello Nikhil.

There are 12 times in TM4C123GH6PM device. On the LP not all pins may have been bond out to the header. If the requirement is to have multiple timers I would suggest using DK-TM4C123G which has the headers for almost all pins to be accessible.

Regards
Amit

 

 

You received this notification because you subscribed to the forum.  To unsubscribe from only this thread, go here.

Flag this post as spam/abuse.