This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL2-RM46 Target Configuration Test failed

Other Parts Discussed in Thread: LAUNCHXL2-RM46

While creating the Target Configuration file for the LAUNCHXL2-RM46 I get the following:

[Start: Texas Instruments XDS110 USB Debug Probe_0]

Execute the command:

%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

/home/safiullah/.ti/ti/0/0/BrdDat/testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 100- or 510-class product.
This utility will load the adapter 'libjioxds110.so'.
The library build date was 'Jul 23 2015'.
The library build time was '19:36:25'.
The library package version is '6.0.14.0'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.

An error occurred while hard opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-260' (0xfffffefc).
The title is 'SC_ERR_XDS110_OPEN'.

The explanation is:
An attempt to connect to the XDS110 failed.
The cause may be one or more of: invalid firmware update, invalid
XDS110 serial number, or faulty USB connection. The firmware and
serial number may be updated using the xdsdfu utility found in
the .../ccs_base/common/uscif/xds110 directory of your
installation. View the ReadMe.txt file there for instructions.

[End: Texas Instruments XDS110 USB Debug Probe_0]

How do I fix this?