Other Parts Discussed in Thread: LM3S811
EKK-LM3S811 Evaluation Kit
In the case that I dont use the on board USB for download, debug or communication .
Is it possible to connect the 3.3V break out pin to an external 3.3 volt source and have the LM3S811 and OLED powered from that ?
The schematics show me that the 5v from the USB is connected to the following :
U6 93C46 ----- VCC and ORG and D0 pull up
U4 FT2232C ----- VCC and RESET pull up
U7 LP3981LD-3.3 ----- IN and VEN