Other Parts Discussed in Thread: HALCOGEN, TMS570LS0432
I've discovered a problem with the SPI settings in HalCoGen.
Setting the SPI mode has no effect in HalCoGen 04.05.00. Using TMS570LS0432 FreeRTOS IAR tools chain.
HalCoGen:
Generates:
/* SPI2 set all pins to functional */
spiREG2->PC0 = (uint32)((uint32)1U << 0U) /* SCS[0] */
| (uint32)((uint32)1U << 9U) /* CLK */
| (uint32)((uint32)1U << 10U) /* SIMO */
| (uint32)((uint32)1U << 11U); /* SOMI */
It does not properly set CS1, CS2 and CS3 to functional
The same goes for SPI3.
I've manually set my pins to functional, so I don't need an answer on how to solve this...It's feedback to the HalCoGen team only.
Best Regards
Henrik Liljedahl