This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Doubt in Tiva C launchpad schematics

Hi, I have a little dumb doubt after cheking the schematics of Tiva C launchpad and it is, what are those H1, H2, H20, H21, H23, H24 etc, marks?? They just appears once on the whole document, and after googling a bit and searching on these forums I couldn't find any clue.


  • Hello Daniel,

    Check which line the header pins are connected to. That will tell what is on the header. E.g. H1 is connected to /HIB signal. So it can be used to check if the device is in Hibernate State or not.

    Regards
    Amit
  • Did you mean to check it on the sheet or in the launchpad?? The thing is, in the document is obvious that H1 is /HIB, but why they mark it as H1?? maybe, have I access to a H1 pin?? I've already check some headers and they doesn't match any pattern (I thought, maybe J1 contains H1-H10 pin headers, J2 H2-h20 and so on) neither are marks such as any HXX on the launchpad board.

    Btw, I have this doubt because there are several pads on the launchpad that are not labeled and I want to know what does pads are for.
  • Hello Daniel,

    OK. Now I get it and you are right. Not all of the points have been marked on the silkscreen. May be I can check up the data base and see if I can post an image on the forum for reference, while we correct the document.

    Regards
    Amit