Other Parts Discussed in Thread: ENERGIA
Hi everyone,
So I got a project where I have to use ethernet.
Well just yesterday I was asking a friend the difference between UDP and TCP packets and how the heck UDP packets make sense for streaming (luckily it's his thing).
For now I am going to use a mix of Energia libraries with Tivaware, hopefully I can get the data rate over 8Mbps with a 10Mbps connection.
But in case it doesn't, or in case I need some extra speed, Tivaware is an option. Problem with the forum, it's really great to see how things can be bad an fail, not common for users to come here "hey this works, it's amazing", so I am bit worried on the stability of both the software and hardware - hence why feedback is welcome :)
I will probably still use the Energia ethernet library but could make some tweaks if it doesn't go right.