This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CAN communication between TMS570LS31x HDK board and TMS570LC43x LaunchPad



I want to establish a communication between TMS570LS31x HDK board and TMS570LC43x LaunchPad board with the CAN interface, can it succeed?

If can, how should I configure both the TMS570LS31x HDK board and TMS570LC43x LaunchPad board?

Expect to a accurate answer.

TKS!

  • Your HDK board has tranceivers. The LaunchPad doesn't.

    You can build a small BoosterPack with a tranceiver. You can use the identical schematic as on the HDK:

    Check page 20. The setup consists of an SN65HVDA541 tranceiver and a few resistors and capacitors.

    On this page you can see how you can connect the tranceivers together (with a termination resistor over the lines at the start and the end of the bus - if you follow the HDK setup, the termination resistors are already part of the schematic):