There is a question.
When I use the TMS570LC43x LaunchPad board, whether I can use DCAN1 communication to DCAN2, which is like using two UARTs to communicate with each other.
If can, how can I connect DCAN1 to DCAN2?
Should I connect DCAN1_Rx to DCAN2_TX and connect DCAN1_Tx to DCAN2_Rx?
Or should I connect DCAN1_Tx to DCAN2_TX and connect DCAN1_Rx to DCAN2_Rx?
Thanks and Regards,
Caven