Other Parts Discussed in Thread: TM4C123GE6PM
Hi everyone,
I have been using Tiva C Launch Pad for sampling a analogic signal and saving the samples in a vector of 128. The code is;
#include <stdint.h>
#include <stdbool.h>
#include <stdlib.h>
#include <time.h>
#include <stdio.h>
#include <math.h>
#include <string.h>
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/debug.h"
#include "driverlib/sysctl.h"
#include "driverlib/adc.h"
#include "driverlib/gpio.h"
#include <tm4c123ge6pm.h>
#include "LaunchPad.h"
int adc [128];
long lBtn1;
long lBtn2;
int main (void) {
uint32_t ADC0Value[1];
volatile uint32_t ui32Loop;
char bDemoState = 0;
SysCtlClockSet(SYSCTL_SYSDIV_10|SYSCTL_USE_PLL|SYSCTL_OSC_MAIN|SYSCTL_XTAL_16MHZ);
SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
GPIOPinTypeGPIOInput(GPIO_PORTD_BASE,GPIO_PIN_2);
GPIOPinTypeADC(GPIO_PORTD_BASE,GPIO_PIN_2);
ADCSequenceConfigure(ADC0_BASE, 3, ADC_TRIGGER_PROCESSOR, 0);
ADCSequenceStepConfigure(ADC0_BASE,3,0,ADC_CTL_CH5|ADC_CTL_IE|ADC_CTL_END);
ADCSequenceEnable(ADC0_BASE, 3);
ADCIntClear(ADC0_BASE, 3);
while(1)
{
for (i=0;i<127;i++){
ADCProcessorTrigger(ADC0_BASE, 3);
while(!ADCIntStatus(ADC0_BASE, 3, false))
{ }
ADCIntClear(ADC0_BASE, 3);
ADCSequenceDataGet(ADC0_BASE,3,ADC0Value);
adc[i]=ADC0Value[0];
}
}
After the line with adc[i]=ADC0Value[0], the breakpoint is disabled; S/W BP- disabled. I can't figure out why. Is the code correct?
My signal has been analogically filtered and is maximum frequency should be around 30 Hz.
Thanks in advance.