Other Parts Discussed in Thread: TMS570LS3137, HALCOGEN
When I use the TMS570LS3137 DCAN interface , how can I configure the TMS570LS3137 DCAN to use many messageboxes to transmit data?
Thanks and Regards,
Caven
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TMS570LS3137, HALCOGEN
When I use the TMS570LS3137 DCAN interface , how can I configure the TMS570LS3137 DCAN to use many messageboxes to transmit data?
Thanks and Regards,
Caven
Hi Caven,
Like Zhaohong said, it is not necessary to use more than one messagebox since it makes no difference to the outside world. It will just help to free the CPU from having to wait too long.
The DCAN uses IF registers to communicate between the DCAN module and the DCAN messageboxes. If you are using HALCoGen, you can just use the canTransmit() API with the required messagebox(the messagebox must be enabled in the HALCoGen GUI).
If you are not using HALCoGen, taking a look at how the canTransmit() is implemented might still help. The configuration of the IFCMD register determines which messagebox will be used for the data passed into the IF register. You can take a look at the TRM for a better understanding(Section DCAN Module -> Message Interface Register Sets -> Using Message Interface Register sets).
Thanks and Regards,
Vineeth