1. This is code which I have written , code goes into hardfault.
SysCtlGPIOAHBEnable(SYSCTL_PERIPH_GPIOF);
while(!(SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOF)));
GPIOPinTypeGPIOOutput(GPIO_PORTF_AHB_BASE, GPIO_PIN_1);
while(1)
{
GPIOPinWrite(GPIO_PORTF_AHB_BASE,GPIO_PIN_1, GPIO_PIN_1);
SysCtlDelay(13333333);
GPIOPinWrite(GPIO_PORTF_AHB_BASE,GPIO_PIN_1, 0);
SysCtlDelay(13333333);
}
2. If I do my APB bus, then no error.
3. Without library it was solved earlier here: