This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UART with the LS31 via USB

Hello everyone,

I have the DRV3801-LS31 Kit and want to use UART-communication for real-time data transmission.
As I understand there is a virtual comport availble on the FT2232H. If I follow the trace on the schematic the
ftdi_scirx and ftdi_scitx signals are not availible to the mcu but are only brought out via the Dimm-100 to a 2-pin jumper (J12).

As i see it, i will not be able to use the USB-UART bridge on the FT2232H with the LS31 MCU. Is this correct?

If so what is the best way to achieve serial, real time data transmission between the PC and the MCU?