This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HET IDE : stimulus creator

When adding a stimulus with a trigger time that is not later than all existing stimuli, it is not displayed at the right position, even when checking the "sort by time" button. It also seems that it is not simulated correctly. Can I file a bug report somewhere?  How can I get the expected behavior?

Thanks,

Daniel Marmier

 

  • Daniel,

    I noticed this myself, but it seems to be a temporary issue.  i.e. if you terminate the simulation and restart, then it'll sort.   Seems to only mis-sort when you first enter the stimulus.

    There's another issue I found w. the stimulus that's worse -- if you enter 'too many' stimulus say 6-8 then they wills start to be dropped.    Should have a release soon that fixes this 2nd issue.

    re.. bug reports - please do exactly what you did and note them here.  

    Thanks and Best Regards,

    Anthony

  • This is exactly the problem that I have : the last ones are dropped.

    About the release : approximately how soon is soon?

    Much thanks and Best Regards,

    Daniel Marmier

  • Daniel,

    It'll be available this month for sure.  

    You might try out using VCD for stimulus in the meantime.  The reason stimulus is dropped from the GUI stimulus editor has to do w. a flaw in the TCP server on the simulator,  but the VCD stimulus would be coming from a file and thus bypass this flaw.