Other Parts Discussed in Thread: UNIFLASH, HALCOGEN, RM48L952, TMS570LS3137
The problem is about HITEX SafeTI-HSK-570LS31-ND that is purchased last week. We could not program (we try to program example project which exists in product’s own DVD and also empty project including HALCoGen assistance) the kit with using CCS or flash tools (uniflash and nowFlash). We get the same error message every time: “Does not match the target endianness, not loaded. Check project build options and target configuration file.” Device endianness selected as be32 because TMS570 supports this format. However, selecting be32, b8, and big produce the same error message, too. Little-endian selection causes compiler error for available example project and meaningless (can be programmed but cannot be achieved any basic functions like lighting a led or sending something via SCI) working for empty project including HALCoGen assistance. Another problem is that D300 Red Led is always lighting which means nRST pin activated, continuously. Additionally, we could not achieve firmware update with using uniflash as it is mentioned in user manual. Just we achieved is erasing flash memory of TMS570 with uniflash. Endianness and nRST problems are mentioned partially in other conversations but there is no valid solution for us, unluckily. We need your assistance, as quickly as possible. Best regards.