Other Parts Discussed in Thread: TM4C129ENCPDT
Hello I am using tivaware 2.1.0.12573c with TM4C129ENCPDT and am finding the I2C module does not appear to be setting busy flag correctly.
If I use a 20ms delay with SysCtlDelay my code reads the FRAM fine, but if I wait for the busy flags to free it doesn't work.
Initialisation code:
// Enable and configure the peripherals used by I2C1
SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C1);
SysCtlPeripheralReset(SYSCTL_PERIPH_I2C1);
GPIOPinConfigure(GPIO_PG1_I2C1SDA);
GPIOPinConfigure(GPIO_PG0_I2C1SCL);
GPIOPinTypeI2CSCL(GPIO_PORTG_BASE, GPIO_PIN_0);
GPIOPinTypeI2C(GPIO_PORTG_BASE, GPIO_PIN_1);
GPIODirModeSet(GPIO_PORTG_BASE, GPIO_PIN_0, GPIO_DIR_MODE_HW);
GPIODirModeSet(GPIO_PORTG_BASE, GPIO_PIN_1, GPIO_DIR_MODE_HW);
I2CMasterInitExpClk(I2C1_BASE, ui32SysClock, true);
HWREG(I2C1_BASE + I2C_O_FIFOCTL) = 80008000;
Reading Code:
//read specified register on slave device
static uint32_t I2CReceive(uint32_t slave_addr, uint8_t reg, uint8_t * rxBuffer, uint16_t size)
{
uint32_t resp;
uint16_t x;
while (I2CMasterBusy(I2C1_BASE));
// SysCtlDelay(ui32SysClock/(20000));
//specify that we are writing (a register address) to the slave device
I2CMasterSlaveAddrSet(I2C1_BASE, slave_addr, false);
I2CMasterDataPut(I2C1_BASE, (reg >> 8) & 0xFF);
I2CMasterControl(I2C1_BASE, I2C_MASTER_CMD_BURST_SEND_START);
while (I2CMasterBusy(I2C1_BASE));
// SysCtlDelay(ui32SysClock/(20000));
I2CMasterDataPut(I2C1_BASE, reg & 0xFF);
I2CMasterControl(I2C1_BASE, I2C_MASTER_CMD_BURST_SEND_FINISH);
while (I2CMasterBusy(I2C1_BASE));
// SysCtlDelay(ui32SysClock/(20000));
x = 0;
//specify that we are going to read from slave device
I2CMasterSlaveAddrSet(I2C1_BASE, slave_addr, true);
if (size == 1)
I2CMasterControl(I2C1_BASE, I2C_MASTER_CMD_SINGLE_RECEIVE);
else
I2CMasterControl(I2C1_BASE, I2C_MASTER_CMD_BURST_RECEIVE_START);
while (x < size)
{
while (I2CMasterBusy(I2C1_BASE));
// SysCtlDelay(ui32SysClock/(20000));
while (HWREG(I2C1_BASE + I2C_O_MCS) & I2C_MCS_BUSY);
resp = I2CMasterDataGet(I2C1_BASE);
rxBuffer[x++] = resp;
if (size > 1 && x < size)
{
while (I2CMasterBusy(I2C1_BASE));
// SysCtlDelay(ui32SysClock/(20000));
if (x < (size - 1))
I2CMasterControl(I2C1_BASE, I2C_MASTER_CMD_BURST_RECEIVE_CONT);
else
I2CMasterControl(I2C1_BASE, I2C_MASTER_CMD_BURST_RECEIVE_FINISH);
}
}
SysCtlDelay(ui32SysClock/(20000));
return 0;
}