Other Parts Discussed in Thread: HALCOGEN, TMS570LS3137, RM48L952, TMS570LS1227
Hey all,
I am a student using the RM4x series for a project. I need to store data that is passed to the controller via CAN until it can be downloaded via a computer. I am looking at storing upwards of 1GB of data total the the course of two hours or so. I know that the RM48 has an EMIF module in HalCoGen but I do not need the memory to store variable values or anything like that, it is just being used as temporary data storage. I am also not concerned with volatility of the memory, the application will be always on. Is there an expected method of interfacing this size external memory or should I just be using GIO and N2HET outputs to do it via a custom driver?
Any pointers would be appreciated!
Nat