This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

GIPO interrrupt on both edges



working with lm4f120h5qr launchpad. want to interface with hcsr04 sensor to launchpad without using "Stellarisware" and other libraries.

my code is as follows :

//This is to avoid doing the math everytime you do a reading
const double temp = 1.0/80.0;

//Stores the pulse length
extern volatile unsigned int pulse;

//Tells the main code if the a pulse is being read at the moment
extern volatile unsigned char echowait;

int main(void)
{

	PLL_Init(); //80mhz
	SysTick_Init();
	Init_Timer();
	Init_sensor();
	
	while(1)
	{
			
    //Checks if a pulse read is in progress
    if(echowait != 1)
			{
				//Does the required pulse of 10uS
				TriggerPulse();
				
					/*This makes the code wait for a reading to finish
					You can omit this part if you want the code to be non-blocking but
					reading is only ready when echowait=0.*/
				
				while(echowait != 0);

				//Converts the counter value to cm.
				pulse =(unsigned int)(temp * pulse);
				pulse = pulse / 58;

				//Prints out the distance measured.
				send_serial("distance = %2dcm \n" , pulse);
			}
      //wait about 10ms until the next reading.
      delay_ms(10);


	}

}
/*********************main end********************/
followinf functions are in different c file : 

volatile unsigned int pulse=0;

volatile unsigned char echowait=0;
void Init_sensor(void) { volatile unsigned long delay; SYSCTL_RCGC2_R |= SYSCTL_RCGC2_GPIOA; // activate clock for port A delay = SYSCTL_RCGC2_R; GPIO_PORTA_AMSEL_R &= ~(TRIG_PIN | ECHO_PIN); // disable analog functionality on PA5,PA6 GPIO_PORTA_PCTL_R |= 0x00222211;//(GPIO_PORTA_PCTL_R&0x00FFFFFF)+0x33000000; // configure PA5 PA6 as GPIO GPIO_PORTA_DIR_R |= TRIG_PIN; // make PA5 out GPIO_PORTA_DIR_R &= ~ECHO_PIN; //make PA6 In //GPIO_PORTA_DR8R_R |= TRIG_PIN; // enable 8 mA drive on PA5,6 GPIO_PORTA_AFSEL_R &= ~(TRIG_PIN | ECHO_PIN); // disable alt funct on PA5,6 GPIO_PORTA_DEN_R = (TRIG_PIN | ECHO_PIN); // enable digital I/O on PA5,6 GPIO_PORTA_PUR_R |= ECHO_PIN; // enable weak pull-up on PA GPIO_PORTA_IS_R &= ~ECHO_PIN; // PA6 is edge-sensitive GPIO_PORTA_IBE_R |= ECHO_PIN; // PA6 is both edges GPIO_PORTA_ICR_R = ECHO_PIN; // clear flags PA6 GPIO_PORTA_IM_R |= ECHO_PIN; // arm interrupt on PA6 NVIC_PRI7_R = (NVIC_PRI7_R&0xFF00FFFF)|0x00400000; // (g) priority 2 NVIC_EN0_R = NVIC_EN0_INT0; // enable interrupt 30 in NVIC } // Start the timers and interrupt frequency void Init_Timer(void) { unsigned long volatile delay; delay = SYSCTL_RCGC2_R; SYSCTL_RCGCTIMER_R |= 0x04; // 0) activate timer2 delay = SYSCTL_RCGC2_R; TIMER2_CTL_R = 0x00000000; // 1) disable timer2A during setup TIMER2_CFG_R = TIMER_CFG_32_BIT_TIMER; // 2) configure for 32-bit mode TIMER2_TAMR_R = TIMER_TAMR_TAMR_PERIOD; // 3) configure for periodic mode, default down-count settings TIMER2_TAILR_R = 0xFFFFFFFF;//((80000000 / 1000000) * 10); // 4) reload value 10us TIMER2_TAPR_R = 0; // 5) bus clock resolution TIMER2_CTL_R = 0x00000001; // enable timer2A }
void EchoPulseHandler(void) //This ISR executes when it detects the end of the echo pulse { unsigned int status = 0; status = GPIO_PORTA_MIS_R; GPIO_PORTA_ICR_R = 0x01; // acknowledge flag0 /* If it's a rising edge then set he timer to 0 It's in periodic mode so it was in some random value */ //if echo pin high means burst is receiv to echo till echo pin gose low if(( status & ECHO_PIN) == ECHO_PIN ) //if high { TIMER2_TAR_R = 0; //Loads value 0 into the timer. TIMER2_CTL_R = 0x00000001; // enable timer2A echowait=1; } // If it's a falling edge that was detected, then get the value of the counter else { pulse = TIMER2_TAV_R; //record value TIMER2_CTL_R = 0x00000000; // disable timer2A echowait=0; } } //This executes the trigger pulse void TriggerPulse(void) { TRIG_PIN_HIGH //Set Trigger pin HIGH delay_us(10); //10us TRIG_PIN_LOW //Set Trigger LOW delay_us(10); //10us } }

1)
the  problem is  falling edge interrupt doesn't occurred , the ISR stuck in raising edge.

i think there is some issue while initialization of port A and ECHO PIN

trigger pin is working ok.

2)

the other thing is when raising edge occurred the counter will be reset but its not.

also i tried   TAV_R but still counter value not reset .


tested  some stellarisware example on the same pins(with PORTA) with sensor , its measure the accurate distance.

  • Hello Forum User

    Classical problem when using the Direct Register Macro's (DRM). Complex code in a few lines and chances of incorrect programming. The Timer TAR is a RO register. You have to use TAILR register for any value load. Configuration of GPIO looks correct. Did you try manually toggling the GPIO using a switch or another GPIO and then see if the MIS bits gets set or not.

    I would strongly urge you to use TivaWare (We know a lot of folks want to learn the processor and hence the DRM).

    Regards
    Amit