Other Parts Discussed in Thread: TM4C123GH6PM
(I previously posted the same question on the wrong forum)
Hello,
I have issues with triggering a Timer2A interrupt on my Tiva TM4C123GXL. I wrote the simple following program to illustrate the issue : 1) the main program sets a flag, 2) it should be interrupted, 3) the ISR should clear the flag, and 4) when back into the main thread the 0 flag should turn the green LED. Instead the red LED turns on (meaning the flag is 1, meaning the interrupt did not clear it, which probably means that the timer2A handler, handlerTimer2A, was not called).
The handler (handlerTimer2A) is initialized in the Interrupt Vector Table, in the startup file (ie 1) declaring : extern void handlerTimer2A (void); and 2) adding handlerTimer2A at vector 39 / IRQ 23 location).
I am aware of other people having similar issues (eg : e2e.ti.com/.../1136794, and I have checked that my problem was not coming from the same causes. Thanks for your help.
Jean
(PS: I follow the lower-level procedure, only for my own educational purpose)
Here is the code :
#include "tm4c123gh6pm.h"
unsigned char flag;
void initportF(void);
void initTimer2A(unsigned long period);
void handlerTimer2A(void){
TIMER2_ICR_R = 0x00000001; // acknowledge
flag = 0; // SET THE FLAG - SHOULD TURN ON THE GREEN LED BACK IN MAIN
TIMER2_CTL_R = 0x00000000; // disable timer2A
}
void main(void){
flag = 1; // INITIALIZE FLAG TO 1
initportF();
initTimer2A(1*80000); // the reload value is not important here
while(1){
if (flag) {GPIO_PORTF_DATA_R = 0x02;} // red LED if flag is 1
else {GPIO_PORTF_DATA_R = 0x08;} // green LED if flag is 0 - which should be the case if the interrupt cleared the flag
}
}
// init Timer2A
void initTimer2A(unsigned long period){
unsigned long volatile delay;
SYSCTL_RCGCTIMER_R |= 0x04; // activate timer2
delay = SYSCTL_RCGCTIMER_R; // wait 3~5 bus cycle
TIMER2_CTL_R = 0x00000000; // disable timer2A
TIMER2_CFG_R = 0x00000000; // 32-bit mode
TIMER2_TAMR_R = 0x00000002; // periodic mode
TIMER2_TAILR_R = period-1; // reload value
TIMER2_TAPR_R = 0; // clock resolution
TIMER2_ICR_R = 0x00000001; // clear timeout flag
TIMER2_IMR_R = 0x00000001; // arm timeout
NVIC_PRI5_R = (NVIC_PRI5_R&0x00FFFFFF)|0x80000000; // priority 4
NVIC_EN0_R = 1<<23; // enable IRQ 23 in
TIMER2_CTL_R = 0x00000001; // enable timer2A
}
// init portF
void initportF(void){
volatile unsigned long delay;
SYSCTL_RCGC2_R |= 0x00000020; // activate clock portF
delay = SYSCTL_RCGC2_R; // wait 3~5 bus cycle
GPIO_PORTF_LOCK_R = 0x4C4F434B; // unlock portF PF0
GPIO_PORTF_CR_R = 0x1F; // allow change PF4,PF3,PF2,PF1,PF0
GPIO_PORTF_DIR_R |= 0x0000000e; // outputs for: PF1(OUTPUT), PF2(OUTPUT), PF3(OUTPUT)
GPIO_PORTF_DIR_R &= ~0x00000011; // inputs for: PF0(INPUT), PF4(INPUT)
GPIO_PORTF_AFSEL_R &= ~0x0000001f; // clear alternative function for: PF0(INPUT), PF4(INPUT), PF1(OUTPUT), PF2(OUTPUT), PF3(OUTPUT)
GPIO_PORTF_DEN_R |= 0x0000001f; // enable digital pins for: PF0(INPUT), PF4(INPUT), PF1(OUTPUT), PF2(OUTPUT), PF3(OUTPUT)
GPIO_PORTF_AMSEL_R &= ~0x0000001f; // disable analog mode for: PF0(INPUT), PF4(INPUT), PF1(OUTPUT), PF2(OUTPUT), PF3(OUTPUT)
GPIO_PORTF_PCTL_R &= ~0x0000001f; // disable PCTL for: PF0(INPUT), PF4(INPUT), PF1(OUTPUT), PF2(OUTPUT), PF3(OUTPUT)
GPIO_PORTF_PUR_R |= 0x00000011; // enable pull-up resistors for: PF0(INPUT), PF4(INPUT)
}