Hello.
I want to use RTI Compare 0 interrupt to trigger ADC in RM46L852PGE chip, without generating RTI interrupts.
Is it possible?
I found that RTICOMP0CLR register is not increased and interrupt flag is not cleared.
/** - Setup compare 0 value. This value is compared with selected free running counter. */
rtiREG1->CMP[0U].COMPx = 1000U;
rtiREG1->CMP[0U].UDCPx = 1000U;
rtiREG1->COMP0CLR = 1500U;
Such simple code lead to correct work RTI Compare 0 module except of interrupt flag setting and not clearing. Register COMP0CLR is not increased.
Why?
Regards,
Vitaliy Bortsov