As part of an FMEA for a system using a TMS570LS04, I need to determine the effects of opening a single VCC or VSS or VCCIO pin.
Do the rest of the pins take up the slack, or is each pin an independent source for a portion of the silicon relying on the PCB for continuity among the pins?
Also, what effects will there be if the FLTP pins are shorted hi or lo?
Thanks