Other Parts Discussed in Thread: RM48L952, HALCOGEN
Hi,
I am using a RM48L952 for UART communication. I am connecting it to a digital tri-axial acceleration sensor. I have to set up an acceleration that seems connected to the GIO port B. When using HALCoGen, and setting up the bit in the GIO Port B, I want to know what everything means. How do I know if the DOUT has to be 0 or 1, also if is has to be input or output. And after that, how can I decide whether is a rising or falling edge, and if it's a high or low priority. I am new to HALCoGen and to microprocessors, but willing to learn.
Thanks!!
Angel