Other Parts Discussed in Thread: RM48L952
Hi There,
I got a strange case on my circuit.vv
I use the RM48l952 ADC for a sample 4-20mA input sampling. The reference voltage is 3V. The input will be 0.54V, 1.08V, 1.62v,2.16v and 2.7V (when input is 4mA,8mA,12mA,16mA and 20mA).
The outpot of the analog circuit is correct when the load is open. The driver is a Emitter follower which can output 8mA current before the ADC's pin of MCU.
When I connect the signal to MCU's pin, the signal became to half level.
Is there someone can tell me the reason. Is there some special requirements for the MCU ADC input?
Thanks,
Chuan..