Other Parts Discussed in Thread: TMS570LC4357, HALCOGEN
Hello,
I have a problem with the EMAC of the TMS570LC4357.
I modified the TMS570LC43x_EMAC_LoopBackMode demo project of halcogen, to send UDP-Packages from the MCU to my Windows-PC (loopbackmode and cache disabled in halcogen). I can see these packages in wireshark. Everything works fine sofar but after 260 packages, the TMS570 always throws a data entry (or data abort) exception.
When I compare the halcogen driver with the requirement for sending packages written in the user manual of ti, I I would say this should be complete and nothing is missing. I did not change anything of the ethernet driver, just configured the payload with ( ip + udp).
I really want a small implementation of the emac-driver, so the lwIP-Demo-Projekt is not a good starting point for me (don't need tcp etc. / footprint to big for my 4 mb flash). I really just want to send simple packages, so please do not simply refer to the lwIP-Demo-Project.
I did also analyse the code of the lwIP-project, but could not find any differences related to the drivers. ( EMACTransmit, hdkif transmit etc ... seems to do the same things)
The solution, I guess should be something simple like clearing a flag or freeing a buffer, but I was not able to find it.
Maybe there is something missing in the driver, which I did not recognize?
-> If I send raw ethernet frames by calling the EMACTransmit(&hdkif_data[0], &pack[0]) function in a loop, I have exactly the same behaviour (data Entry exception in HL_sys_intvecs.asm)
I read nearly any post and comment about the EMAC in this community but did not find anything that could help me. This is the reason why I post this question now.
Does anyone of you use this MCU and Ethernet and could help me please?
Thank's for your help, already in advance!
Only for your interest: I am receiving FlexRay data on the TMS570 and want to put it into ethernet packages and forward it to my pc on which a software will visualize the data.