Im using the Tiva4c129 to 120 MHz, also im using the SSi0 but the problem is that the maximum speed that i can configure is 60 MHZ in master mode, so my question, is there any form that i can upgrade the CLK of 120 MHZ to a faster one like 250MHz or something like that to have more frequency on SSI0 in master mode?