The question is about SafeTI-HSK-570LS31-ND safety kit. I have already checked the suggested forum posts but could not get the related answer.
ENDRV pin is always LOW and it measures as 0.01 V. The necessary test code is achieved by using SafeTI Diagnostic Library 2.2.0 and I also checked the configuration from the following link.
http://processors.wiki.ti.com/index.php/Configuring_HALCoGen_for_using_TPS_Driver
I also checked the NRES pin then I measured it as 3.3 V. For this reason, it can be said that TPS65381 is not in Standby State or Reset State. Actually, according to our observations, TPS65381 enters Diagnostic State at first, then it enters Active State.
Both in Diagnostic or Active states, state of the ENDRV pin is determined by the Watchdog Fail Count value. Additionally, ENABLE_DRV and WD_RST_EN are set as true and false, respectively as default.
Probably, we miss some crucial point. We will be thankful if you give detailed information about state and working concept of the ENDRV pin.
Best Regards.