I am trying to use the microcontroller to do a few things: 1) sample a sine wave input at PD0 using ADC0 on Timer1 interrupt 2) output that same data to a DAC using SSI0 on Timer1 as well, and 3) continually flash an LED at 2 Hz. I have a functioning simpler version of the code which still outputs to a DAC through SSI0, but lacks ADC functionality. As soon as I try to use ADC0, the CCS debug tells me it is having errors connecting to GPIOF (LEDs are no longer flashing), both TIMER0 and TIMER1, and SSI0 (every function I tried to use). This i supposed to be a fairly simple exercise, so I think the mistake(s) I am making are probably simple but I don't know where to look. If someone could point me in the right direction, that would be great.
#include <stdint.h> // Variable definitions for the C99 standard. #include <stdio.h> // Input and output facilities for the C99 standard. #include <stdbool.h> // Boolean definitions for the C99 standard. #include <math.h> #include "inc/tm4c123gh6pm.h" // Definitions for the interrupt and register assignments. #include "inc/hw_memmap.h" // Memory map definitions of the Tiva C Series device. #include "inc/hw_types.h" // Definitions of common types and macros. #include "inc/hw_ssi.h" #include "driverlib/sysctl.h" // Definitions and macros for System Control API of DriverLib. #include "driverlib/interrupt.h" // Defines and macros for NVIC Controller API of DriverLib. #include "driverlib/gpio.h" // Definitions and macros for GPIO API of DriverLib. #include "driverlib/timer.h" // Defines and macros for Timer API of DriverLib. #include "driverlib/pin_map.h" //Mapping of peripherals to pins for all parts. #include "driverlib/uart.h" // Definitions and macros for UART API of DriverLib. #include "driverlib/fpu.h" // Prototypes for the FPU manipulation routines. #include "driverlib/ssi.h" // Definitions and prototypes for the SSI/SPI routines. #include "driverlib/adc.h" // Definitions for ADC API of DriverLib. #include "utils/uartstdio.h" // Prototypes for the UART console functions. // Needs to add "utils/uartstdio.c" through a relative link. #define TIMER0_FREQ 2 // Freqency in Hz, heartbeat timer #define UART0_BAUDRATE 115200 // UART baudrate in bps #define ADC0_SEQ_NUM 0 // ADC Sample Sequence Number #define SAMP_FREQ 16000 // Frequency in Hz, common sampling rates for digital audio: 44100, 48000 #define SIG_FREQ 1000 // Signal frequency in Hz. #define SIG_LEN 16 // = SAMP_FREQ/SIG_FREQ, period of discrete-time signal #define SPI_BITRATE 15000000 // needs to > SAMP_FREQ*16, and < SysCtrlClock/2, max 20M #define SPI_DATA_MASK 0x0FFF // See datasheet, MCP4921 #define SPI_CTRL_MASK 0x7000 // See datasheet, MCP4921 #define MATH_PI 3.14159265358979323846 #define RED_LED GPIO_PIN_1 #define BLUE_LED GPIO_PIN_2 #define GREEN_LED GPIO_PIN_3 #define NUM_DISP_TEXT_LINE 4 // function prototypes void init_ADC(void); void init_LEDs(void); void init_timer(void); void init_UART(void); void init_SPI(void); void init_signal(void); void Timer0_ISR(void); void Timer1_ISR(void); extern void UARTStdioIntHandler(void); // global variables uint8_t cur_LED = RED_LED; const char *disp_text[NUM_DISP_TEXT_LINE] = { "\n", "UART and LED Demo\n", "H: help, R: red, G: green, B: blue.\n", "> " }; uint16_t sig[SIG_LEN], sig_index=0; uint32_t sys_clock; uint32_t ANALOG_INPUT = 0; int main(void) { uint32_t i; unsigned char user_cmd; SysCtlClockSet(SYSCTL_SYSDIV_2_5|SYSCTL_USE_PLL|SYSCTL_XTAL_16MHZ|SYSCTL_OSC_MAIN); // 80 MHz sys_clock = 80000000; // Hard-coded for 80MHz because of a bug in SysCtlClockGet(). // Enable the floating-point unit (FPU). FPUEnable(); // Configure FPU to perform lazy stacking of the floating-point state. FPULazyStackingEnable(); init_ADC(); init_LEDs(); init_UART(); init_timer(); init_SPI(); init_signal(); // Enable the processor to respond to interrupts. IntMasterEnable(); // Start the timer by enabling operation of the timer module. TimerEnable(TIMER0_BASE, TIMER_A); TimerEnable(TIMER1_BASE, TIMER_A); // Initial display on terminal. for(i=0; i<NUM_DISP_TEXT_LINE; i++) UARTprintf(disp_text[i]); while(1) { // Read user inputs from UART if available. if(UARTRxBytesAvail()) user_cmd = UARTgetc(); else user_cmd = 0; switch(user_cmd){ case '\r': case ' ': case 'H': case 'h': for(i=0; i<NUM_DISP_TEXT_LINE; i++) UARTprintf(disp_text[i]); break; case 'R': case 'r': cur_LED = RED_LED; UARTprintf("\n> "); break; case 'B': case 'b': cur_LED = BLUE_LED; UARTprintf("\n> "); break; case 'G': case 'g': cur_LED = GREEN_LED; UARTprintf("\n> "); break; } } } void init_ADC(void) { // Enable and configure ADC0 SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0); GPIOPinTypeADC(GPIO_PORTD_BASE, GPIO_PIN_0); ADCSequenceConfigure(ADC0_BASE, ADC0_SEQ_NUM, ADC_TRIGGER_PROCESSOR, 0); ADCSequenceStepConfigure(ADC0_BASE, ADC0_SEQ_NUM, 0, ADC_CTL_CH7 | ADC_CTL_IE | ADC_CTL_END ); ADCSequenceEnable(ADC0_BASE, ADC0_SEQ_NUM); ADCIntEnable(ADC0_BASE, ADC0_SEQ_NUM); } void init_LEDs(void) { // Enable and configure LED peripheral. SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF); // Enable GPIO Port F. // Three onboard LEDs, R:PF1, B:PF2, G:PF3. GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3); } void init_timer(void) { // Enable and configure Timer0 peripheral. SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0); // Configure as a 32-bit timer in periodic mode. TimerConfigure(TIMER0_BASE, TIMER_CFG_PERIODIC); // Initialize timer load register. TimerLoadSet(TIMER0_BASE, TIMER_A, sys_clock/TIMER0_FREQ -1); // Registers a function to be called when the interrupt occurs. IntRegister(INT_TIMER0A, Timer0_ISR); // The specified interrupt is enabled in the interrupt controller. IntEnable(INT_TIMER0A); // Enable the indicated timer interrupt source. TimerIntEnable(TIMER0_BASE, TIMER_TIMA_TIMEOUT); // Enable and configure Timer1 peripheral. SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER1); // Configure as a 32-bit timer in periodic mode. TimerConfigure(TIMER1_BASE, TIMER_CFG_PERIODIC); // Initialize timer load register. TimerLoadSet(TIMER1_BASE, TIMER_A, sys_clock/SAMP_FREQ -1); // Registers a function to be called when the interrupt occurs. IntRegister(INT_TIMER1A, Timer1_ISR); // The specified interrupt is enabled in the interrupt controller. IntEnable(INT_TIMER1A); // Enable the indicated timer interrupt source. TimerIntEnable(TIMER1_BASE, TIMER_TIMA_TIMEOUT); } void init_UART(void) { // Enable and configure UART0 for debugging printouts. SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0); SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA); GPIOPinConfigure(GPIO_PA0_U0RX); GPIOPinConfigure(GPIO_PA1_U0TX); GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1); // Registers a function to be called when the interrupt occurs. IntRegister(INT_UART0, UARTStdioIntHandler); UARTStdioConfig(0, UART0_BAUDRATE, sys_clock); } void init_SPI(void) { // Enable peripheral for SSI/SPI. SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA); SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI0); // Configure the muxing and GPIO settings to bring the SSI/SPI functions out to the pins // PA2: SSI0CLK, PA3: SSI0FSS, PA5: SSI0TX GPIOPinConfigure(GPIO_PA2_SSI0CLK); GPIOPinConfigure(GPIO_PA3_SSI0FSS); GPIOPinConfigure(GPIO_PA5_SSI0TX); GPIOPinTypeSSI(GPIO_PORTA_BASE, GPIO_PIN_2|GPIO_PIN_3|GPIO_PIN_5); SSIConfigSetExpClk(SSI0_BASE, sys_clock, SSI_FRF_MOTO_MODE_0, SSI_MODE_MASTER, SPI_BITRATE, 16); SSIEnable(SSI0_BASE); } // Initialize signal table void init_signal(void) { uint32_t i; float w; w = 2*MATH_PI*SIG_FREQ/SAMP_FREQ; for(i=0; i<SIG_LEN; i++) { sig[i] = 0x0FFF*(1 + sinf(w*i))/2; sig[i] = SPI_CTRL_MASK | (SPI_DATA_MASK & sig[i]); } } // Timer0 interrupt service routine void Timer0_ISR(void) { // Clear the timer interrupt. TimerIntClear(TIMER0_BASE, TIMER_TIMA_TIMEOUT); // Blink LED. Read the current state of GPIO pins and write back the opposite state. if(GPIOPinRead(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3)) { GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3, 0); } else { GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3, cur_LED); } } // Timer1 interrupt service routine void Timer1_ISR(void) { // Clear the timer interrupt. TimerIntClear(TIMER1_BASE, TIMER_TIMA_TIMEOUT); // Sample data from PD0 ADCProcessorTrigger(ADC0_BASE, ADC0_SEQ_NUM); while(!ADCIntStatus(ADC0_BASE, ADC0_SEQ_NUM, false)) { } ADCIntClear(ADC0_BASE, ADC0_SEQ_NUM); ADCSequenceDataGet(ADC0_BASE, ADC0_SEQ_NUM, &ANALOG_INPUT); // Send data to SPI. SSIDataPut(SSI0_BASE, sig[sig_index]); if(sig_index < SIG_LEN-1) sig_index++; else sig_index = 0; }
Thank you