Other Parts Discussed in Thread: HALCOGEN
Hello,
I'm using the RM48L952ZWT with the TMDSRM48HDK dev board.
My goal is to transfer data via the USB Device port (J16) to my laptop using Windows 7 64.
I'm following this instruction:
http://processors.wiki.ti.com/index.php/HALCoGen_USB_Device_-_driver_&_CDC_Class
to set up HalcoGen correctly.
The first question that I have is about the USB clock, after reading this post:
https://e2e.ti.com/support/microcontrollers/hercules/f/312/t/369302
looks like VCLKA3_DIVR should be set to 12MHz, dividing 48Mhz by 4, but in the instruction page above it doesn't mention it and shows VCLKA_DIVR and VCLKA(_S) both at 48 Mhz. What is the correct clock setting?
An other thing is that in the instruction page, about the VIM RAM setting, there is the setup for the interrupt service routine for the USBD where serviceIrq is assigned from vector 68 to 72 but then on the VIM Channel 64-95 Tab only interrupt 69 and 70 are enabled and not 68,71,72. Is this correct?
I had configured HalCogen as per instruction above and used the file example_usbd_cdc.c in the C:\ti\Hercules\HALCoGen\v04.05.01\examples\RM48x\example_usbd_cdc to complete the main file.
As the instruction page suggest, Windows can't find the driver for the Virtual COM port (as in the picture)
So I follow the instruction on how to locate it, but when I provide the folder where the inf file is (same folder as the example_usbd_cdc.c file, the inf file is usb_dev_serial.inf) Windows complain the was unable to find driver software for the device.
Please let me know if you think i'm doing something wrong.
Thanks again
Giorgio