I want to use this microcontroller, but i want to know which MAXCLOCK SPI or MAXCLOCK SSI that i can configure,i want tho use a SPI memory ( that work at 108 MHZ in single mode) to save the raw data(bits) of a image sensor(that works at 6MHz to 96MHz), so i need to know the MAXCLOCK limit of this microcontroller