This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I saw a prior post from 6 weeks ago. Is there any solution to running the Launchpad ICDI USB drivers under Windows 10? I am stuck until I get that fixed.
I got the drivers to install.
The trick is turning off driver signing. The information on the web is pretty sketchy and the mechanism has changed recently. There are lots of Win8 examples, but not many for Win/10.
The procedure I used:
OR, replace steps 1-3 with this:
Then follow the normal procedure to update/install the driver. You will get a message verifying you want to install a non-signed driver.
I hope this helps others
Hi Amit,
i tried the way in this post. However, windows driver still can't be installed properly. Could you please tell me do we have windows driver for win10? thank you
Hello Lisa
Did you try the TivaWare 2.1.4 driver files.These have been signed
Hi,
I downloaded SW-TM4C-2.1.4.178.exe and installed it and plugged in my TIVA hardware. The device manager shows a warning on "Device Firmware Upgrade" so I updated the driver and pointed "C:\ti\TivaWare_C_Series-2.1.4.178\windows_drivers" as shown below
I then click next and it tries to load the driver but fails with the following message
If I turn off driver device checking (using the suggestions at the top of this post) then it does install and work.
Can you please confirm 2.1.4 are actually signed.
cheers
Chris