This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Hibernation Interrupt I/O



why is it when i debug, the tiva board starts to hibernate?
Also, how do i set the timing for LED to 1 min?
void HibernateHandler(void) {
uint32_t ui32Status;
// // Get the interrupt status, and clear any pending interrupts. //
ui32Status = HibernateIntStatus(1);
HibernateIntClear(ui32Status);
// // Process the RTC match 0 interrupt. //
if(ui32Status & HIBERNATE_INT_RTC_MATCH_0) {
GPIOPinWrite(GPIO_PORTF_BASE,GPIO_PIN_3, GPIO_PIN_3);
}
}
int main(void)
{
SysCtlClockSet(SYSCTL_SYSDIV_5|SYSCTL_USE_PLL|SYSCTL_XTAL_16MHZ|SYSCTL_OSC_MAIN);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3);
GPIOPinWrite(GPIO_PORTF_BASE,GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3, 0x08);
SysCtlPeripheralEnable(SYSCTL_PERIPH_HIBERNATE);
HibernateEnableExpClk(SysCtlClockGet());
HibernateGPIORetentionEnable();
SysCtlDelay(64000000);
HibernateRTCSet(0);
HibernateRTCEnable();
HibernateRTCMatchSet(0,HibernateRTCGet()+60);
HibernateWakeSet(HIBERNATE_WAKE_PIN | HIBERNATE_WAKE_RTC);
GPIOPinWrite(GPIO_PORTF_BASE,GPIO_PIN_3, 0x00);
HibernateIntEnable(HIBERNATE_INT_RTC_MATCH_0);
HibernateIntClear(HIBERNATE_INT_PIN_WAKE | HIBERNATE_INT_LOW_BAT | HIBERNATE_INT_RTC_MATCH_0);
//HibernateIntRegister(HibernateHandler);
HibernateRequest();
while(1)
{
}
}

void HibernateHandler(void) { uint32_t ui32Status; // // Get the interrupt status, and clear any pending interrupts. // ui32Status = HibernateIntStatus(1); HibernateIntClear(ui32Status); // // Process the RTC match 0 interrupt. // if(ui32Status & HIBERNATE_INT_RTC_MATCH_0) { GPIOPinWrite(GPIO_PORTF_BASE,GPIO_PIN_3, GPIO_PIN_3); }}
int main(void){ SysCtlClockSet(SYSCTL_SYSDIV_5|SYSCTL_USE_PLL|SYSCTL_XTAL_16MHZ|SYSCTL_OSC_MAIN); SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF); GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3); GPIOPinWrite(GPIO_PORTF_BASE,GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3, 0x08); SysCtlPeripheralEnable(SYSCTL_PERIPH_HIBERNATE); HibernateEnableExpClk(SysCtlClockGet()); HibernateGPIORetentionEnable(); SysCtlDelay(64000000); HibernateRTCSet(0); HibernateRTCEnable(); HibernateRTCMatchSet(0,HibernateRTCGet()+60); HibernateWakeSet(HIBERNATE_WAKE_PIN | HIBERNATE_WAKE_RTC); GPIOPinWrite(GPIO_PORTF_BASE,GPIO_PIN_3, 0x00);
HibernateIntEnable(HIBERNATE_INT_RTC_MATCH_0); HibernateIntClear(HIBERNATE_INT_PIN_WAKE | HIBERNATE_INT_LOW_BAT | HIBERNATE_INT_RTC_MATCH_0); //HibernateIntRegister(HibernateHandler);
HibernateRequest(); while(1) {
}}void HibernateHandler(void) { uint32_t ui32Status; // // Get the interrupt status, and clear any pending interrupts. // ui32Status = HibernateIntStatus(1); HibernateIntClear(ui32Status); // // Process the RTC match 0 interrupt. // if(ui32Status & HIBERNATE_INT_RTC_MATCH_0) { GPIOPinWrite(GPIO_PORTF_BASE,GPIO_PIN_3, GPIO_PIN_3); }}
int main(void){ SysCtlClockSet(SYSCTL_SYSDIV_5|SYSCTL_USE_PLL|SYSCTL_XTAL_16MHZ|SYSCTL_OSC_MAIN); SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF); GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3); GPIOPinWrite(GPIO_PORTF_BASE,GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3, 0x08); SysCtlPeripheralEnable(SYSCTL_PERIPH_HIBERNATE); HibernateEnableExpClk(SysCtlClockGet()); HibernateGPIORetentionEnable(); SysCtlDelay(64000000); HibernateRTCSet(0); HibernateRTCEnable(); HibernateRTCMatchSet(0,HibernateRTCGet()+60); HibernateWakeSet(HIBERNATE_WAKE_PIN | HIBERNATE_WAKE_RTC); GPIOPinWrite(GPIO_PORTF_BASE,GPIO_PIN_3, 0x00);
HibernateIntEnable(HIBERNATE_INT_RTC_MATCH_0); HibernateIntClear(HIBERNATE_INT_PIN_WAKE | HIBERNATE_INT_LOW_BAT | HIBERNATE_INT_RTC_MATCH_0); //HibernateIntRegister(HibernateHandler);
HibernateRequest(); while(1) {
}}