Other Parts Discussed in Thread: LM3S6911, LM3S6965, LM3S2110, LM3S8962
Hi,This is my 1st post, so, excuse if it sound stupid...
we are ready to develop PCB board using LM3S6911.
I could not find enough information to complete the schematic.
I planing to use the EKT-LM3S6955 to program/debug my 'going to be developed board'
My development tool will be Code-Red.
My question,
Can anyone please provide example schematic which has the following;
1. programmable via EKT-LM3S6955 evaluation kit
2. UART Port(Rs-232, 115Kbps)
3. Interface to SD card (micro)
4. I2C line connected to DS1307+ (RTC chip)
5. LAN Interface (recommended suitable magnetic)
6. 10-GPIO
I can take care the regulator, reset, crystal, 232 line interface and other external module.
I need support on which pin/port need to be used on the above requirement.
I know what I am asking to a lot, you assistance is highly appreciated and when you are in Malaysia, I take you for beer... ;-)