This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Why GPIOPinConfigure versus GPIODirModeSet to assign GPIO pin to named AFSEL peripheral.

Guru 56308 points

Other Parts Discussed in Thread: EK-TM4C1294XL, LM3S8971, TM4C1294NCPDT

Some confusion why there is a GPIOPinConfigur() when GPIODirModeSet() appears both can set GPIO pin to assign HW peripheral?

Never do see GPIOPinConfigure() being used in any TI software, seems to be deprecated or redundant.

 

 

  • Hello BP101,

    GPIOPinConfigure is there. Please check the drivers/pinout.c file in EK-TM4C1294XL

    Regards
    Amit
  • Hi Amit,

    Yes indeed it is but why?

    GPIODirModeSet() seems to do the same function selecting the MUX pin for as a peripheral in AFSEL via HW direction.
  • Hello BP101

    GPIOPinConfigure sets the PCTL value.

    Regards
    Amit
  • Hi Amit / CB1

    Data sheet GPIO Register 22 0x52c most bits in the GPIOAFSEL are GPIO ports by default after POR. That explains why we don't see GPIOPinConfigure() being used after setting the GPIODirModeSet() with IN or OUT.

    That changes when an peripheral other than GPIO is desired. Then both are required to set the GPIO pin Mux to the specific peripheral Port pin. Most all the GPIOPinTypeXXXXXX() driver lib commands are not setting REG 22 peripheral because most are GPIO related pin assignments in the GPIOAFSEL. Never connected the dots in the past being it most always was a GPIO port pin selection those times and ADC/PWM configure are calling GPIOPinConfigure(). The problem occurs when there is no library command to set a alternate peripheral function to an external pin it has to be done manually in three steps.

    Been trying for long time to select the PWM0 external fault pin 71 on the LM3S8971. Now setting AFSEL 0x420 HW direction followed by setting REG22  0x52c via GPIOPinConfigure(FAULT_PERIPH).

    Why is this not working?

    // Make GPIO PB3 Pin71 the PWM0 fault input (AFSEL).
       GPIODirModeSet(GPIO_PORTB_BASE, GPIO_PIN_3, GPIO_DIR_MODE_HW);
    // Set PB3 with a weak pull down for the PWM0 fault input.
       GPIOPadConfigSet(GPIO_PORTB_BASE, GPIO_PIN_3, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD_WPD);
    // Configure the peripheral (REG22 0x52c) signal for pin 71 
       GPIOPinConfigure(FAULT_PERIPH);

  • Hello BP101,

    What is the value of FAULT_PERIPH?

    Regards
    Amit
  • Hi Amit,

    It eventually ends up being (SYSCTL_PERIPH_GPIOB 0x20000002). So it seems after adding very last step GPIOPinConfigure() pin 71 now asserts PWM cut off but was difficult to confirm and causes an LWIP problem.

    The problem asserting pin 71 creates remains even after clearing legacy PWMfault0 and disabling PWM0 INT 25. If pin 71 remains high during INT25 handler the EMAC/PHY LWIP timers slow down so much the GUI refuses to connect TCP.

    Is there a GPIOPinToggle() function in driverlib that will pulse the GPIO pin versus writing it?
  • Hello BP101

    The parameter to the GPIOPinConfigure is defined in the file pin_map.h in driverlib. It must be one of the Pin Port Value defines in this file.

    Regards
    Amit
  • Hi Amit,
    Yes that is where #define FAULT_PERIPH is located and translates to SYSCTL_PERIPH_GPIOB cross names again over to SYSCTL_PERIPH_GPIOB.

    Pin 71 is getting configured now but was acting very strange using ADC_Trigger_PWM0 would not work with more than one FIFO sequencer.

    Is it considered a violation to use the ADC_Trigger_PWM0 to start simultaneous samples (IE, END) in 2 or all 4 FIFO sample sequencers?
  • Hello BP101.

    No. It should be something like GPIO_PB3_MxFAULTy

    Secondly which device are you using, and which Fault Pin ?

    Regards
    Amit
  • Hi Amit,
    Was back tracking the LM3s8971 PWM0 fault pin 71 input and migration of SW into TM4C. That was Stellaris driverlib 10636 PB3 drive pin 71.
  • Hello BP101,

    Assuming that it TM4C1294NCPDT PWM Fault 0 Pin, the define must be GPIO_PF4_M0FAULT0.

    Regards
    Amit
  • BP101 said:
    Hi Amit / CB1

    You perchance - rang?

    Was locked out from the forum for past 4 hours - just now was (allowed) to log in.

    Here's the code which enabled our setting of the PWM Fault input - this for LX4F under Stellaris 9453.  (last ver. which supported LX4F)

         ROM_GPIOPinTypePWM(GPIO_PORTF_BASE, GPIO_PIN_2);
         ROM_GPIOPinConfigure(GPIO_PF2_M0FAULT0);      

  • Hi CB1 & Amit

    Thanks, seems that one is completely different name for LM3S8971.

    PWM0 fault pin is confirmed working. The problem was compare 2 integers <> a given sample value. The CPU was running over 121% when first started to debug that compare code to determine the ADC sample values.

    New method code compare  (top) stops continuous true. The old method below that stopped working after moving the ADC_Trigger_Processor out of the called function. That may be why Trigger_PWM0 was also not working with ADC0 SS2. Unclear is PWM fault INT 25 was not firing or NVIC would not allow it to. SS2 and PWM0_Fault had the same priority level 0x40 and SS2 has a higher interrupt number seems to have violated the priority rule. In that case the lower interrupt should of had priority at least in the TM4C world priority group 4.

     if(g_ulAnalogVoltage < 9457 > 9739) //stops continuous true
    
     if((g_ulAnalogVoltage < 9457) || (g_ulAnalogVoltage > 9739)) //true all the time

  • Hello BP101

    So there was another problem on top of the "incorrectly" configured pin.

    Regards
    Amit
  • Hi Amit,

    Good to know the GPIO mux pin register (GPIOPinConfigure()) needs to be configured ever a pin changed direction HW that by default is GPIO SW mode. Seems redundant pad mux is not more intuitive in that 2 registers have to be programmed in that case. Possibly the DEN bit LM3S was not OR'd with the peripheral pin selection. So when the HW direct, AFSEL modes were set that did not automatically set the GPIO pin mux to reflect the change. We had to then call GPIOPinConfigure() to set REG22 0x52c GPIOPCTL.

    Question: TM4C analog comparator digital output pins are not by default SW control GPIO mode? Tivaware GPIOPinTypeComparatorOutput() does not call GPIOPinConfigure() after setting the direction mode to HW. The output of the analog comparator is (digital) requires to set REG18 GPIODEN bit 1?

    There is no TM4C GPIO default pin mode table in the datasheet as in LM3S data sheet. Without that table in the LM3S would never have put it together Pin71 was by default SW mode. TI/Tiva PinMux tools makes the very same assumptions. Perhaps a yellow high light GPIO pins that default to SW mode on POR might shed some light on what code is required beyond what is being automated.

  • Hello BP101

    To be on the same context: The device we are referring to is the TM4C129x. The GPIOPinTypeComparatorOutput does not call and does not need to call GPIOPinConfigure. These two API's are separate and must be called by the application.

    Regards
    Amit
  • Hi Amit,

    >"GPIOPinTypeComparatorOutput does not call and does not need to call GPIOPinConfigure"

    But why --- stated in TM4C1294 datasheet (yellow) most pins default to GPIO SW mode. You knew I was going to ask that question.

    I know GPIOPinConfigure() is a separate call in Tivaware. How do we know when to call GPIOPinConfigure() -- by what (table) in the data sheet leads us to that deduction? Seems Tiva PinMux tools is only doing half what is required, for example programming the digital comparator output it negates GPIOPinConfiure() for what ever reason. It seems GPIOPinConfigure() is required by what the datasheet states below.

    Table (10-4 GPIO pin examples) may be missing a GPIOPCTL column (reference 10.3.3) that would help to clarify if for example the digital comparator output, we also need to call GPIOPinCOnfigure() in the application.  GPIODirModeSet() sets AFSEL 0x420- and with HW mode DIR 0x400 but does not set GPIOPCTL REG22 0x52C set in GPIOPinConfigure() which must be set when ever AFSEL is selected.

    Register 22: GPIO Port Control (GPIOPCTL), offset 0x52C
    The GPIOPCTL register is used in conjunction with the GPIOAFSEL register and selects the specific
    peripheral signal for each GPIO pin when using the alternate function mode. Most bits in the
    GPIOAFSEL register are cleared on reset, therefore most GPIO pins are configured as GPIOs by
    default. When a bit is set in the GPIOAFSEL register, the corresponding GPIO signal is controlled
    by an associated peripheral. The GPIOPCTL register selects one out of a set of peripheral functions
    for each GPIO, providing additional flexibility in signal definition.

  • Sorry Amit,

    Tiva PinMux tool did add GPIOPinConfigure() for the analog comparator digital outputs. Seems it must call it after all.

    But it didn't call GPIOPinConfigure() for the analog comparator inputs.

  • Hello BP101

    Note that Tiva Pin Mux is replaced by the TI Pin Mux Tool. Also another important item to note that Analog pins do not need GPIOPinConfigure as it is not GPIOPCTL based

    Regards
    Amit
  • Hi Amit,

    >" Analog pins do not need GPIOPinConfigure as it is not GPIOPCTL based"

    So table 10-4 shows us the analog comparator input is default AFSEL 0, DEN 0 and Table 10-4 is not just an example rather the POR defaults table?

    But then again the analog comparators have digital outputs and use a GPIO port pin for the SW mode of the peripheral. Table 10-4 shows that AFSEL 1, DEN 1 so we use GPIOPinConfigure() only for the digital output? Seems to me all analog inputs start out as GPIO default SW mode until the direction is changed to HW but how does the GPIO pad know that unless we issue GPIOPinConfigure()? Many Tivaware driverlib calls state it must be called after the GPIO pin assignment. 

    That is why a table is needed to visually show GPIO pins default mode SW or HW as text states (most GPIO pins). Just what does the word most imply is debatable. Seems you take the word most to excluded all analog input pins that share a GPIO port pin. Where in the datasheet is it clearly stated that certain GPIO pins are not by default GPIO in SW mode after POR?   

    Naming table 10-4 "GPIO Pad Configuration Examples" is not exactly confirming certain pins don't fall under the (most) GPIO pin SW mode category on POR. Seems to me Table 10-4 shows the required configurations for peripheral modes that share GPIO pins and that (may or may not) default to SW mode on POR. Who really knows, table 10-4 shows only the required configurations not the default POR configurations. 

    Then we have this claim that seems to infer we always call GPIOPinCOnfigure after changing peripheral direction to HW.

    GPIOPinConfigure:

    //! Configures the alternate function of a GPIO pin.
    //!
    //! \param ulPinConfig is the pin configuration value, specified as only one of
    //! the \b GPIO_P??_??? values.
    //!
    //! This function configures the pin mux that selects the peripheral function
    //! associated with a particular GPIO pin.  Only one peripheral function at a
    //! time can be associated with a GPIO pin, and each peripheral function should
    //! only be associated with a single GPIO pin at a time (despite the fact that
    //! many of them can be associated with more than one GPIO pin). To fully
    //! configure a pin, a GPIOPinType*() function should also be called. 

  • Hi Amit,

    REG22: When a bit is set in the GPIOAFSEL register, the corresponding GPIO signal is controlled
    by an associated peripheral. Always true????????

    Basically any time the GPIO pin direction is changed to HW, above statement is (supposed) to be true.

    Case LM3S8971 PWM0 GPIO PB3 Fault Pin71 did not automatically follow the PWM0 peripheral module. That only occurred after GPIOPinConfigure assigned GPIO PB3 to the peripheral. That is why I remain skeptical with TM4C when changing the analog comparator direction to HW, GPIOPinTypeComparator() perhaps should be followed by GPIOPinConfigure?

    We have to keep consistent in the rules or make certain our tables explain deviations from the typical (most) pattern.
  • Hi Amit,

    The GPIOPCTL register selects one out of a set of peripheral functions for each GPIO, providing additional flexibility in signal definition.

    What is considered (the set of functions) of a peripheral that require GPIOPinConfigure or what BITS confirm when to call it.

    Does the GPIO assigned analog comparator inputs fall under that same category of peripheral functions. Perhaps when DEN=0, AFSEL=0 exclude all  peripheral owned functions shown in Table 10-4? Simply saying that the comparator input/output pin is analog makes no sense when using the datasheet table 10-4 or simply reading the Tivaware Doxygen text. Seems plausible to call (GPIOPinConfigure) in all cases when the datasheet is not handy to confirm its proper use.

    More simply:

    AFSEL=1, DEN=1, GPIOPCTL=1 :GPIOPinConfigure is required?

    AFSEL=0, DEN=0, GPIOPCTL=X :GPIOPinConfigure is Not required?

  • Hello BP101

    Yes. Note that the second part of the statement is "GPIO signal is controlled by an associated peripheral". The Associated peripheral is decided by the PCTL register.

    Regards
    Amit
  • Hello BP101

    DEN=1 is required both for Peripheral and GPIO control. However the GPIOPinTypeXXX takes care of AFSEL and DEN in this case.

    Regards
    Amit
  • Hi Amit,

    >the corresponding GPIO signal is controlled by an associated peripheral. {"Only after GPIOPCTL has been set does the associated GPIO pin become linked to the peripheral" is missing in the text.}

    To me statement and table 10-4 as it is written in datasheet infers when ever any GPIO peripheral has been selected via AFSEL=1 or DEN=1, the associated GPIO port pins of that peripheral are automatically assigned because they are controlled by association. Controlled by the associated peripheral infers the peripheral owns the GPIO port pins without doing anything further.

    That is why table 10-4 might benefit to help clarify that missing controlled associativity by including a GPIOPCTL column.
  • Hello BP101

    The issue is that there are more than one PCTL value that could be possible for a peripheral to control the pin. And this would vary from device to device. Thus the Table 26-5 adds more clarity to what the GPIO Pin and its alternate functions available.

    Regards
    Amit
  • Hi Amit,

    Understand reasoning for not listing each and every PCTL mux value in the column. That don't mean we can't associate a (true/false/x=don't care)  column in table 10-4 to indicate register 22 presence. At the very least add more clarity to the text so people don't believe the peripheral owns the GPIO pin after the AFSEL association is changed to HW mode. That becomes especially relevant in the wording that (most) bits in the AFSEL default to GPIO SW mode. Again that misleads to modify association only have to change AFSEL/DEN bits. Seems someone at TI purposefully went out of their way to make changing GPIO pin ownership overly complicated where simplicity was the intended goal.

    You have shed light on what was interpreted as completely different peripheral behavior.

    Many thanks! :)

  • Hello BP101,

    Argument accepted. Yes, it can add clarity to the table. I will try to push in the change when the data sheet revision is scheduled.

    Regards
    Amit