This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ethernet interface to ROM boot loader and Flash boot loader source for the TM4C1294NCPDT



A quick Google search immediately returned a link to documentation for the TivaWare Boot Loader, but I have been unable to find the actual source. Based on forum posts I learned that that documentation only applies to the Flash version of the boot loader, which should only be used when the ROM version is missing a required feature. The ROM boot loader cannot be modified and ships with some TI MCUs.

Reading the documentation for my processor does mention a ROM based boot loader and the TivaWare Peripheral Driver Library discusses interfacing with ROM, but not over Ethernet. Is there a way to interface with the ROM boot loader over Ethernet?

Either way, where can I find the source for the Flash based boot loader? I've done extensive searching, including the following obvious locations: