Other Parts Discussed in Thread: TM4C1294NCZAD
According to the datasheet for the Tiva C microcontroller, EPI0 and USB0 external PHY signals collided with each other. Especially EPI016, EPI017, EPI018, EPI019, EPI026, EPI027, EPI028, EPI033 with USB0[0..5], USB0STP, USB0CLK.
Can I assign different EPI signals to configure SDRAM other than the ones specified in the datasheet and how do i configure them?. For example, TM4C1294nczad section 11.4.2.1 External Signal Connections for SDRAM. I need both external SDRAM and high speed USB PHY on the same PCB.