This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357 - pinmux options and features



Dear all,

I would like to ask you for clarifying a few issues regarding pinmux setting.

1) Preliminary question

Is it possible to change the pinmux setting more times (e.g. periodically) during the run-time?

  • I guess that is allowed - only the locking mechanism must be applied (to write 2 lock values - magic constants).
  • Anyway I have in my mind this procedure is not allowed and the pinmux can be set only once during the run-time (e.g. at the start-up). But I have not found any restriction like this within the Safety Manual SPNU540 May 2014.

According to the TRM SPNU563 May 2014 (chapter 6.6.1 Locking Mechanism for Memory-Mapped Registers), the answer seems to be YES...

2) Scenario

Our intention is to use the BGA balls (terminals):

  • V2: for both signals N2HET1[1] as well as eQEP2A - both as input ones
  • U1: for both signals N2HET1[3] as well as eQEP2B - both as input ones

During the run-time the both signals from the terminal V2 will be processed (by NHET and eQEP module) - in the sequence (periodically "switched" or switching based on the Condition A - see below), not simultaneously

If the Condition A is true, the input signal on the terminal V2 will be "connected" to (processed by) NHET module.

If the Condition A is false, the input signal on the terminal V2 will be "connected" to (processed by) eQEP module.

Similar situation is applied for the terminal U1.

3) Alternative solution

According to the TRM SPNU563 May 2014 (the NOTE below Table 6-2. Input Multiplexing and Control on 337ZWT Package):

Inputs are broadcast to all multiplexed functions
The input signals are broadcast to all modules hooked up to a terminal.

So does this NOTE mean that the periodical pinmux switching (discussed in 1)) is NOT necessary? An application must decide (e.g. according to the mentioned Condition A) whether the input signal on the terminal V2 will be processed by NHET module or by eQEP module?

Thanks for your explanation,

Best regards, Jiri

  • Hi Jiri,

    Your understanding is correct. " the periodical pinmux switching (discussed in 1)) is NOT necessary? An application must decide (e.g. according to the mentioned Condition A) whether the input signal on the terminal V2 will be processed by NHET module or by eQEP module?"

    1) It is possible to change pinmuxing at run-time.

    3) Multiple Module input pins(eg: N2HET1[1] and eQEP2A ) can be connected to a single ball(V2) simultaneously and process the signal at the same time.

    Thanks and Regards,
    Vineeth

     

  • Hi Vineeth,

    thanks a lot for your quick and clear answer!

    Well, we are happy from the functional view. Furthermore I would like to ask you for confirmation that we will not breach any safety rule regarding the pinmuxing etc. if we use this feature and behavior.
    As I mentioned I had not found any restriction in the Safety Manual SPNU540 May 2014. But there is a huge amount of the documentation I could have missed anything...

    Thanks,
    Best regards, Jiri
  • Hi Jiri,

    I'm not an expert on safety and am not aware of any such rule. I'll try to ask around to see if something like that is available. In the mean time we can wait for other posters' views.

    Thanks and Regards,
    Vineeth

  • Hi Jiri,

    There should be no safety concern related to this scenario. You can go ahead.

    Thanks and Regards,
    Vineeth