This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C123GH6PMI in Tiva C Series Launchpad Silicon Revision



Hello, I have a board with the microcontroller Tiva TM4C123GH6PMI, but does not clarify the silicon review.

At the top of the CI he says:

Line 1: 980 YF

Line 2: TM4C123G

Line 3: 41AXE8W

Line 4; G4 (underlined)

The board is EX-TM4C123GXL Rev A

I'm using Keil 5.16a. And the latest libraries TivaWare the date of writing this question (TivaWare_C_Series-2.1.0.12573).

#define TARGET_IS_TM4C123_RB1 ?????? Is this correct?, or should use TARGET_IS_BLIZZARD_RB1
#include "driverlib/rom.h"
#include "driverlib/rom_map.h"

Thanks!