This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

while(ROM_SSIBusy(SSI3_BASE)) delay

Hi all,

I am interfacing DAC1220 and ADS1256 to TM4C1290 microcontroller. I am using ADS1256 at 500SPS. i want to update DAC output when i get the ADC interrupt means almost at 2 mSec.

Please find code below for DAC output.

 

void DAC_SPI_Transmit(unsigned char temp_spi1_array[],unsigned char total_bytes)
{
unsigned char delay_i=0;

if(Peripheral_Fail[DAC] == 0)
{
for (delay_i=0;delay_i<total_bytes;delay_i++)
{
ROM_SSIDataPut(SSI3_BASE,temp_spi1_array[delay_i]);

Peripherals_Check_Timeout = 0;
while(ROM_SSIBusy(SSI3_BASE))
{
if(Peripherals_Check_Timeout > 2)
{
Peripheral_Fail[DAC] = 1;
return;
}
}

ROM_SSIDataGet(SSI3_BASE, (uint32_t *)&rcvd_data[0]);
}
}
else
return;
}

Now the problem is ROM_SSIDataPut(SSI3_BASE,temp_spi1_array[delay_i]); and while(ROM_SSIBusy(SSI3_BASE)) take too much time that i cant update DAC in 2 mSec. Can you provide delay information for these two functions?