Other Parts Discussed in Thread: TM4C129ENCPDT, EK-TM4C1294XL
I am using a TM4C129ENCPDT processor with tirtos_tivac_2_12_01_33
The USB is interfacing to a Ublox Toby modem.
I am finding that the USB for the PPP port seems to get out of synch with the modem.
By out of synch I mean that I see no responses from the modem for a period of 1 to 2 minutes and then it starts responding but to my earlier messages.
A normal AT port works fine, just the port on which I have had a PPP session active seems to fail.
Doing a reset on the modem itself doesn't resolve the issue.
Doing a reset of my entire board does resolve the issue.
This seems to indicate I either have a hardware or software issue within the USB interface.
Interestingly the working AT port is part of the same device enumeration, only the PPP port behaves strangely.
I was wondering if there is a way of Resetting the USB host stack so it starts from default when I reset the modem.