This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

What relationship between DMA transfer and UART transfer in example project udma_demo project?



Hi,

I am new to these new Tiva micro-controller. I learn Uart example project udma_demo, which is part of TivaWare_C_Series-2.1.1.71, on TM4C1294 LaunchPad. It has Uart with dma transfer. It also says software initiates DMA transfer in the code comments. On reading the code, I see DMA uses memory  g_ui32SrcBuf, g_ui32DstBuf in:

ROM_uDMAChannelTransferSet(UDMA_CHANNEL_SW, UDMA_MODE_AUTO,
g_ui32SrcBuf, g_ui32DstBuf,
MEM_BUFFER_SIZE);

The above DMA transfers data from memory g_ui32SrcBuf to g_ui32DstBuf?

I don't see the above DMA transfers date to UART explicitly. DMA channel for UART is another DMA?

I see g_ui8RxBufA and g_ui8RxBufB in UART1IntHandler():

ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART1RX | UDMA_PRI_SELECT,
UDMA_MODE_PINGPONG,
(void *)(UART1_BASE + UART_O_DR),
g_ui8RxBufA, sizeof(g_ui8RxBufA));
}

I don't see the memory contents connection between g_ui8RxBufA(or g_ui8RxBufB) with g_ui32SrcBuf or g_ui32DstBuf. 

There is a DMA enable function inside InitUART1Transfer(void):

ROM_uDMAChannelEnable(UDMA_CHANNEL_UART1RX);
ROM_uDMAChannelEnable(UDMA_CHANNEL_UART1TX);

The example project shows CPU usage on DMA transfers data. What role is for UART?

Could you explain it to me? The memory transferred by UART1IntHandler(void) has connection with that of uDMAIntHandler(void)?

Thanks,

//*****************************************************************************
//
// The interrupt handler for uDMA interrupts from the memory channel.  This
// interrupt will increment a counter, and then restart another memory
// transfer.
//
//*****************************************************************************
void
uDMAIntHandler(void)
{
    uint32_t ui32Mode;

    //
    // Check for the primary control structure to indicate complete.
    //
    ui32Mode = ROM_uDMAChannelModeGet(UDMA_CHANNEL_SW);
    if(ui32Mode == UDMA_MODE_STOP)
    {
        //
        // Increment the count of completed transfers.
        //
        g_ui32MemXferCount++;

        //
        // Configure it for another transfer.
        //
        ROM_uDMAChannelTransferSet(UDMA_CHANNEL_SW, UDMA_MODE_AUTO,
                                     g_ui32SrcBuf, g_ui32DstBuf,
                                     MEM_BUFFER_SIZE);

        //
        // Initiate another transfer.
        //
        ROM_uDMAChannelEnable(UDMA_CHANNEL_SW);
        ROM_uDMAChannelRequest(UDMA_CHANNEL_SW);
    }

    //
    // If the channel is not stopped, then something is wrong.
    //
    else
    {
        g_ui32BadISR++;
    }
}

//*****************************************************************************
//
// The interrupt handler for UART1.  This interrupt will occur when a DMA
// transfer is complete using the UART1 uDMA channel.  It will also be
// triggered if the peripheral signals an error.  This interrupt handler will
// switch between receive ping-pong buffers A and B.  It will also restart a TX
// uDMA transfer if the prior transfer is complete.  This will keep the UART
// running continuously (looping TX data back to RX).
//
//*****************************************************************************
void
UART1IntHandler(void)
{
    uint32_t ui32Status;
    uint32_t ui32Mode;

    //
    // Read the interrupt status of the UART.
    //
    ui32Status = ROM_UARTIntStatus(UART1_BASE, 1);

    //
    // Clear any pending status, even though there should be none since no UART
    // interrupts were enabled.  If UART error interrupts were enabled, then
    // those interrupts could occur here and should be handled.  Since uDMA is
    // used for both the RX and TX, then neither of those interrupts should be
    // enabled.
    //
    ROM_UARTIntClear(UART1_BASE, ui32Status);

    //
    // Check the DMA control table to see if the ping-pong "A" transfer is
    // complete.  The "A" transfer uses receive buffer "A", and the primary
    // control structure.
    //
    ui32Mode = ROM_uDMAChannelModeGet(UDMA_CHANNEL_UART1RX | UDMA_PRI_SELECT);

    //
    // If the primary control structure indicates stop, that means the "A"
    // receive buffer is done.  The uDMA controller should still be receiving
    // data into the "B" buffer.
    //
    if(ui32Mode == UDMA_MODE_STOP)
    {
        //
        // Increment a counter to indicate data was received into buffer A.  In
        // a real application this would be used to signal the main thread that
        // data was received so the main thread can process the data.
        //
        g_ui32RxBufACount++;

        //
        // Set up the next transfer for the "A" buffer, using the primary
        // control structure.  When the ongoing receive into the "B" buffer is
        // done, the uDMA controller will switch back to this one.  This
        // example re-uses buffer A, but a more sophisticated application could
        // use a rotating set of buffers to increase the amount of time that
        // the main thread has to process the data in the buffer before it is
        // reused.
        //
        ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART1RX | UDMA_PRI_SELECT,
                                   UDMA_MODE_PINGPONG,
                                   (void *)(UART1_BASE + UART_O_DR),
                                   g_ui8RxBufA, sizeof(g_ui8RxBufA));
    }

    //
    // Check the DMA control table to see if the ping-pong "B" transfer is
    // complete.  The "B" transfer uses receive buffer "B", and the alternate
    // control structure.
    //
    ui32Mode = ROM_uDMAChannelModeGet(UDMA_CHANNEL_UART1RX | UDMA_ALT_SELECT);

    //
    // If the alternate control structure indicates stop, that means the "B"
    // receive buffer is done.  The uDMA controller should still be receiving
    // data into the "A" buffer.
    //
    if(ui32Mode == UDMA_MODE_STOP)
    {
        //
        // Increment a counter to indicate data was received into buffer A.  In
        // a real application this would be used to signal the main thread that
        // data was received so the main thread can process the data.
        //
        g_ui32RxBufBCount++;

        //
        // Set up the next transfer for the "B" buffer, using the alternate
        // control structure.  When the ongoing receive into the "A" buffer is
        // done, the uDMA controller will switch back to this one.  This
        // example re-uses buffer B, but a more sophisticated application could
        // use a rotating set of buffers to increase the amount of time that
        // the main thread has to process the data in the buffer before it is
        // reused.
        //
        ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART1RX | UDMA_ALT_SELECT,
                                   UDMA_MODE_PINGPONG,
                                   (void *)(UART1_BASE + UART_O_DR),
                                   g_ui8RxBufB, sizeof(g_ui8RxBufB));
    }

    //
    // If the UART1 DMA TX channel is disabled, that means the TX DMA transfer
    // is done.
    //
    if(!ROM_uDMAChannelIsEnabled(UDMA_CHANNEL_UART1TX))
    {
        //
        // Start another DMA transfer to UART1 TX.
        //
        ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART1TX | UDMA_PRI_SELECT,
                                   UDMA_MODE_BASIC, g_ui8TxBuf,
                                   (void *)(UART1_BASE + UART_O_DR),
                                   sizeof(g_ui8TxBuf));

        //
        // The uDMA TX channel must be re-enabled.
        //
        ROM_uDMAChannelEnable(UDMA_CHANNEL_UART1TX);
    }
}

//*****************************************************************************
//
// Initializes the UART1 peripheral and sets up the TX and RX uDMA channels.
// The UART is configured for loopback mode so that any data sent on TX will be
// received on RX.  The uDMA channels are configured so that the TX channel
// will copy data from a buffer to the UART TX output.  And the uDMA RX channel
// will receive any incoming data into a pair of buffers in ping-pong mode.
//
//*****************************************************************************
void
InitUART1Transfer(void)
{
    uint_fast16_t ui16Idx;

    //
    // Fill the TX buffer with a simple data pattern.
    //
    for(ui16Idx = 0; ui16Idx < UART_TXBUF_SIZE; ui16Idx++)
    {
        g_ui8TxBuf[ui16Idx] = ui16Idx;
    }

    //
    // Enable the UART peripheral, and configure it to operate even if the CPU
    // is in sleep.
    //
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART1);
    ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_UART1);

    //
    // Configure the UART communication parameters.
    //
    ROM_UARTConfigSetExpClk(UART1_BASE, g_ui32SysClock, 115200,
                            UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
                            UART_CONFIG_PAR_NONE);

    //
    // Set both the TX and RX trigger thresholds to 4.  This will be used by
    // the uDMA controller to signal when more data should be transferred.  The
    // uDMA TX and RX channels will be configured so that it can transfer 4
    // bytes in a burst when the UART is ready to transfer more data.
    //
    ROM_UARTFIFOLevelSet(UART1_BASE, UART_FIFO_TX4_8, UART_FIFO_RX4_8);

    //
    // Enable the UART for operation, and enable the uDMA interface for both TX
    // and RX channels.
    //
    ROM_UARTEnable(UART1_BASE);
    ROM_UARTDMAEnable(UART1_BASE, UART_DMA_RX | UART_DMA_TX);

    //
    // This register write will set the UART to operate in loopback mode.  Any
    // data sent on the TX output will be received on the RX input.
    //
    HWREG(UART1_BASE + UART_O_CTL) |= UART_CTL_LBE;

    //
    // Put the attributes in a known state for the uDMA UART1RX channel.  These
    // should already be disabled by default.
    //
    ROM_uDMAChannelAttributeDisable(UDMA_CHANNEL_UART1RX,
                                    UDMA_ATTR_ALTSELECT | UDMA_ATTR_USEBURST |
                                    UDMA_ATTR_HIGH_PRIORITY |
                                    UDMA_ATTR_REQMASK);

    //
    // Configure the control parameters for the primary control structure for
    // the UART RX channel.  The primary contol structure is used for the "A"
    // part of the ping-pong receive.  The transfer data size is 8 bits, the
    // source address does not increment since it will be reading from a
    // register.  The destination address increment is byte 8-bit bytes.  The
    // arbitration size is set to 4 to match the RX FIFO trigger threshold.
    // The uDMA controller will use a 4 byte burst transfer if possible.  This
    // will be somewhat more effecient that single byte transfers.
    //
    ROM_uDMAChannelControlSet(UDMA_CHANNEL_UART1RX | UDMA_PRI_SELECT,
                              UDMA_SIZE_8 | UDMA_SRC_INC_NONE | UDMA_DST_INC_8 |
                              UDMA_ARB_4);

    //
    // Configure the control parameters for the alternate control structure for
    // the UART RX channel.  The alternate contol structure is used for the "B"
    // part of the ping-pong receive.  The configuration is identical to the
    // primary/A control structure.
    //
    ROM_uDMAChannelControlSet(UDMA_CHANNEL_UART1RX | UDMA_ALT_SELECT,
                              UDMA_SIZE_8 | UDMA_SRC_INC_NONE | UDMA_DST_INC_8 |
                              UDMA_ARB_4);

    //
    // Set up the transfer parameters for the UART RX primary control
    // structure.  The mode is set to ping-pong, the transfer source is the
    // UART data register, and the destination is the receive "A" buffer.  The
    // transfer size is set to match the size of the buffer.
    //
    ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART1RX | UDMA_PRI_SELECT,
                               UDMA_MODE_PINGPONG,
                               (void *)(UART1_BASE + UART_O_DR),
                               g_ui8RxBufA, sizeof(g_ui8RxBufA));

    //
    // Set up the transfer parameters for the UART RX alternate control
    // structure.  The mode is set to ping-pong, the transfer source is the
    // UART data register, and the destination is the receive "B" buffer.  The
    // transfer size is set to match the size of the buffer.
    //
    ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART1RX | UDMA_ALT_SELECT,
                               UDMA_MODE_PINGPONG,
                               (void *)(UART1_BASE + UART_O_DR),
                               g_ui8RxBufB, sizeof(g_ui8RxBufB));

    //
    // Put the attributes in a known state for the uDMA UART1TX channel.  These
    // should already be disabled by default.
    //
    ROM_uDMAChannelAttributeDisable(UDMA_CHANNEL_UART1TX,
                                    UDMA_ATTR_ALTSELECT |
                                    UDMA_ATTR_HIGH_PRIORITY |
                                    UDMA_ATTR_REQMASK);

    //
    // Set the USEBURST attribute for the uDMA UART TX channel.  This will
    // force the controller to always use a burst when transferring data from
    // the TX buffer to the UART.  This is somewhat more effecient bus usage
    // than the default which allows single or burst transfers.
    //
    ROM_uDMAChannelAttributeEnable(UDMA_CHANNEL_UART1TX, UDMA_ATTR_USEBURST);

    //
    // Configure the control parameters for the UART TX.  The uDMA UART TX
    // channel is used to transfer a block of data from a buffer to the UART.
    // The data size is 8 bits.  The source address increment is 8-bit bytes
    // since the data is coming from a buffer.  The destination increment is
    // none since the data is to be written to the UART data register.  The
    // arbitration size is set to 4, which matches the UART TX FIFO trigger
    // threshold.
    //
    ROM_uDMAChannelControlSet(UDMA_CHANNEL_UART1TX | UDMA_PRI_SELECT,
                              UDMA_SIZE_8 | UDMA_SRC_INC_8 |
                              UDMA_DST_INC_NONE |
                              UDMA_ARB_4);

    //
    // Set up the transfer parameters for the uDMA UART TX channel.  This will
    // configure the transfer source and destination and the transfer size.
    // Basic mode is used because the peripheral is making the uDMA transfer
    // request.  The source is the TX buffer and the destination is the UART
    // data register.
    //
    ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART1TX | UDMA_PRI_SELECT,
                               UDMA_MODE_BASIC, g_ui8TxBuf,
                               (void *)(UART1_BASE + UART_O_DR),
                               sizeof(g_ui8TxBuf));

    //
    // Now both the uDMA UART TX and RX channels are primed to start a
    // transfer.  As soon as the channels are enabled, the peripheral will
    // issue a transfer request and the data transfers will begin.
    //
    ROM_uDMAChannelEnable(UDMA_CHANNEL_UART1RX);
    ROM_uDMAChannelEnable(UDMA_CHANNEL_UART1TX);

    //
    // Enable the UART DMA TX/RX interrupts.
    //
    ROM_UARTIntEnable(UART1_BASE, UART_INT_DMATX | UART_INT_DMATX);

    //
    // Enable the UART peripheral interrupts.
    //
    ROM_IntEnable(INT_UART1);
}

//*****************************************************************************
//
// udma_demo.c - uDMA example.
//
// Copyright (c) 2013-2015 Texas Instruments Incorporated.  All rights reserved.
// Software License Agreement
// 
// Texas Instruments (TI) is supplying this software for use solely and
// exclusively on TI's microcontroller products. The software is owned by
// TI and/or its suppliers, and is protected under applicable copyright
// laws. You may not combine this software with "viral" open-source
// software in order to form a larger program.
// 
// THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
// NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
// NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
// CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
// DAMAGES, FOR ANY REASON WHATSOEVER.
// 
// This is part of revision 2.1.1.71 of the EK-TM4C1294XL Firmware Package.
//
//*****************************************************************************

#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "inc/hw_uart.h"
#include "driverlib/fpu.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/rom_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/systick.h"
#include "driverlib/uart.h"
#include "driverlib/udma.h"
#include "utils/cpu_usage.h"
#include "utils/uartstdio.h"
#include "utils/ustdlib.h"

//*****************************************************************************
//
//! \addtogroup example_list
//! <h1>uDMA (udma_demo)</h1>
//!
//! This example application demonstrates the use of the uDMA controller to
//! transfer data between memory buffers, and to transfer data to and from a
//! UART.  The test runs for 10 seconds before exiting.
//!
//! UART0, connected to the ICDI virtual COM port and running at 115,200,
//! 8-N-1, is used to display messages from this application.
//
//*****************************************************************************

//****************************************************************************
//
// System clock rate in Hz.
//
//****************************************************************************
uint32_t g_ui32SysClock;

//*****************************************************************************
//
// The number of SysTick ticks per second used for the SysTick interrupt.
//
//*****************************************************************************
#define SYSTICKS_PER_SECOND     100

//*****************************************************************************
//
// The size of the memory transfer source and destination buffers (in words).
//
//*****************************************************************************
#define MEM_BUFFER_SIZE         1024

//*****************************************************************************
//
// The size of the UART transmit and receive buffers.  They do not need to be
// the same size.
//
//*****************************************************************************
#define UART_TXBUF_SIZE         256
#define UART_RXBUF_SIZE         256

//*****************************************************************************
//
// The source and destination buffers used for memory transfers.
//
//*****************************************************************************
static uint32_t g_ui32SrcBuf[MEM_BUFFER_SIZE];
static uint32_t g_ui32DstBuf[MEM_BUFFER_SIZE];

//*****************************************************************************
//
// The transmit and receive buffers used for the UART transfers.  There is one
// transmit buffer and a pair of recieve ping-pong buffers.
//
//*****************************************************************************
static uint8_t g_ui8TxBuf[UART_TXBUF_SIZE];
static uint8_t g_ui8RxBufA[UART_RXBUF_SIZE];
static uint8_t g_ui8RxBufB[UART_RXBUF_SIZE];

//*****************************************************************************
//
// The count of uDMA errors.  This value is incremented by the uDMA error
// handler.
//
//*****************************************************************************
static uint32_t g_ui32uDMAErrCount = 0;

//*****************************************************************************
//
// The count of times the uDMA interrupt occurred but the uDMA transfer was not
// complete.  This should remain 0.
//
//*****************************************************************************
static uint32_t g_ui32BadISR = 0;

//*****************************************************************************
//
// The count of UART buffers filled, one for each ping-pong buffer.
//
//*****************************************************************************
static uint32_t g_ui32RxBufACount = 0;
static uint32_t g_ui32RxBufBCount = 0;

//*****************************************************************************
//
// The count of memory uDMA transfer blocks.  This value is incremented by the
// uDMA interrupt handler whenever a memory block transfer is completed.
//
//*****************************************************************************
static uint32_t g_ui32MemXferCount = 0;

//*****************************************************************************
//
// The CPU usage in percent, in 16.16 fixed point format.
//
//*****************************************************************************
static uint32_t g_ui32CPUUsage;

//*****************************************************************************
//
// The number of seconds elapsed since the start of the program.  This value is
// maintained by the SysTick interrupt handler.
//
//*****************************************************************************
static uint32_t g_ui32Seconds = 0;

//*****************************************************************************
//
// The control table used by the uDMA controller.  This table must be aligned
// to a 1024 byte boundary.
//
//*****************************************************************************
#if defined(ewarm)
#pragma data_alignment=1024
uint8_t pui8ControlTable[1024];
#elif defined(ccs)
#pragma DATA_ALIGN(pui8ControlTable, 1024)
uint8_t pui8ControlTable[1024];
#else
uint8_t pui8ControlTable[1024] __attribute__ ((aligned(1024)));
#endif

//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif

//*****************************************************************************
//
// The interrupt handler for the SysTick timer.  This handler will increment a
// seconds counter whenever the appropriate number of ticks has occurred.  It
// will also call the CPU usage tick function to find the CPU usage percent.
//
//*****************************************************************************
void
SysTickHandler(void)
{
    static uint32_t ui32TickCount = 0;

    //
    // Increment the tick counter.
    //
    ui32TickCount++;

    //
    // If the number of ticks per second has occurred, then increment the
    // seconds counter.
    //
    if(!(ui32TickCount % SYSTICKS_PER_SECOND))
    {
        g_ui32Seconds++;
    }

    //
    // Call the CPU usage tick function.  This function will compute the amount
    // of cycles used by the CPU since the last call and return the result in
    // percent in fixed point 16.16 format.
    //
    g_ui32CPUUsage = CPUUsageTick();
}

//*****************************************************************************
//
// The interrupt handler for uDMA errors.  This interrupt will occur if the
// uDMA encounters a bus error while trying to perform a transfer.  This
// handler just increments a counter if an error occurs.
//
//*****************************************************************************
void
uDMAErrorHandler(void)
{
    uint32_t ui32Status;

    //
    // Check for uDMA error bit
    //
    ui32Status = ROM_uDMAErrorStatusGet();

    //
    // If there is a uDMA error, then clear the error and increment
    // the error counter.
    //
    if(ui32Status)
    {
        ROM_uDMAErrorStatusClear();
        g_ui32uDMAErrCount++;
    }
}

//*****************************************************************************
//
// The interrupt handler for uDMA interrupts from the memory channel.  This
// interrupt will increment a counter, and then restart another memory
// transfer.
//
//*****************************************************************************
void
uDMAIntHandler(void)
{
    uint32_t ui32Mode;

    //
    // Check for the primary control structure to indicate complete.
    //
    ui32Mode = ROM_uDMAChannelModeGet(UDMA_CHANNEL_SW);
    if(ui32Mode == UDMA_MODE_STOP)
    {
        //
        // Increment the count of completed transfers.
        //
        g_ui32MemXferCount++;

        //
        // Configure it for another transfer.
        //
        ROM_uDMAChannelTransferSet(UDMA_CHANNEL_SW, UDMA_MODE_AUTO,
                                     g_ui32SrcBuf, g_ui32DstBuf,
                                     MEM_BUFFER_SIZE);

        //
        // Initiate another transfer.
        //
        ROM_uDMAChannelEnable(UDMA_CHANNEL_SW);
        ROM_uDMAChannelRequest(UDMA_CHANNEL_SW);
    }

    //
    // If the channel is not stopped, then something is wrong.
    //
    else
    {
        g_ui32BadISR++;
    }
}

//*****************************************************************************
//
// The interrupt handler for UART1.  This interrupt will occur when a DMA
// transfer is complete using the UART1 uDMA channel.  It will also be
// triggered if the peripheral signals an error.  This interrupt handler will
// switch between receive ping-pong buffers A and B.  It will also restart a TX
// uDMA transfer if the prior transfer is complete.  This will keep the UART
// running continuously (looping TX data back to RX).
//
//*****************************************************************************
void
UART1IntHandler(void)
{
    uint32_t ui32Status;
    uint32_t ui32Mode;

    //
    // Read the interrupt status of the UART.
    //
    ui32Status = ROM_UARTIntStatus(UART1_BASE, 1);

    //
    // Clear any pending status, even though there should be none since no UART
    // interrupts were enabled.  If UART error interrupts were enabled, then
    // those interrupts could occur here and should be handled.  Since uDMA is
    // used for both the RX and TX, then neither of those interrupts should be
    // enabled.
    //
    ROM_UARTIntClear(UART1_BASE, ui32Status);

    //
    // Check the DMA control table to see if the ping-pong "A" transfer is
    // complete.  The "A" transfer uses receive buffer "A", and the primary
    // control structure.
    //
    ui32Mode = ROM_uDMAChannelModeGet(UDMA_CHANNEL_UART1RX | UDMA_PRI_SELECT);

    //
    // If the primary control structure indicates stop, that means the "A"
    // receive buffer is done.  The uDMA controller should still be receiving
    // data into the "B" buffer.
    //
    if(ui32Mode == UDMA_MODE_STOP)
    {
        //
        // Increment a counter to indicate data was received into buffer A.  In
        // a real application this would be used to signal the main thread that
        // data was received so the main thread can process the data.
        //
        g_ui32RxBufACount++;

        //
        // Set up the next transfer for the "A" buffer, using the primary
        // control structure.  When the ongoing receive into the "B" buffer is
        // done, the uDMA controller will switch back to this one.  This
        // example re-uses buffer A, but a more sophisticated application could
        // use a rotating set of buffers to increase the amount of time that
        // the main thread has to process the data in the buffer before it is
        // reused.
        //
        ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART1RX | UDMA_PRI_SELECT,
                                   UDMA_MODE_PINGPONG,
                                   (void *)(UART1_BASE + UART_O_DR),
                                   g_ui8RxBufA, sizeof(g_ui8RxBufA));
    }

    //
    // Check the DMA control table to see if the ping-pong "B" transfer is
    // complete.  The "B" transfer uses receive buffer "B", and the alternate
    // control structure.
    //
    ui32Mode = ROM_uDMAChannelModeGet(UDMA_CHANNEL_UART1RX | UDMA_ALT_SELECT);

    //
    // If the alternate control structure indicates stop, that means the "B"
    // receive buffer is done.  The uDMA controller should still be receiving
    // data into the "A" buffer.
    //
    if(ui32Mode == UDMA_MODE_STOP)
    {
        //
        // Increment a counter to indicate data was received into buffer A.  In
        // a real application this would be used to signal the main thread that
        // data was received so the main thread can process the data.
        //
        g_ui32RxBufBCount++;

        //
        // Set up the next transfer for the "B" buffer, using the alternate
        // control structure.  When the ongoing receive into the "A" buffer is
        // done, the uDMA controller will switch back to this one.  This
        // example re-uses buffer B, but a more sophisticated application could
        // use a rotating set of buffers to increase the amount of time that
        // the main thread has to process the data in the buffer before it is
        // reused.
        //
        ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART1RX | UDMA_ALT_SELECT,
                                   UDMA_MODE_PINGPONG,
                                   (void *)(UART1_BASE + UART_O_DR),
                                   g_ui8RxBufB, sizeof(g_ui8RxBufB));
    }

    //
    // If the UART1 DMA TX channel is disabled, that means the TX DMA transfer
    // is done.
    //
    if(!ROM_uDMAChannelIsEnabled(UDMA_CHANNEL_UART1TX))
    {
        //
        // Start another DMA transfer to UART1 TX.
        //
        ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART1TX | UDMA_PRI_SELECT,
                                   UDMA_MODE_BASIC, g_ui8TxBuf,
                                   (void *)(UART1_BASE + UART_O_DR),
                                   sizeof(g_ui8TxBuf));

        //
        // The uDMA TX channel must be re-enabled.
        //
        ROM_uDMAChannelEnable(UDMA_CHANNEL_UART1TX);
    }
}

//*****************************************************************************
//
// Initializes the UART1 peripheral and sets up the TX and RX uDMA channels.
// The UART is configured for loopback mode so that any data sent on TX will be
// received on RX.  The uDMA channels are configured so that the TX channel
// will copy data from a buffer to the UART TX output.  And the uDMA RX channel
// will receive any incoming data into a pair of buffers in ping-pong mode.
//
//*****************************************************************************
void
InitUART1Transfer(void)
{
    uint_fast16_t ui16Idx;

    //
    // Fill the TX buffer with a simple data pattern.
    //
    for(ui16Idx = 0; ui16Idx < UART_TXBUF_SIZE; ui16Idx++)
    {
        g_ui8TxBuf[ui16Idx] = ui16Idx;
    }

    //
    // Enable the UART peripheral, and configure it to operate even if the CPU
    // is in sleep.
    //
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART1);
    ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_UART1);

    //
    // Configure the UART communication parameters.
    //
    ROM_UARTConfigSetExpClk(UART1_BASE, g_ui32SysClock, 115200,
                            UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
                            UART_CONFIG_PAR_NONE);

    //
    // Set both the TX and RX trigger thresholds to 4.  This will be used by
    // the uDMA controller to signal when more data should be transferred.  The
    // uDMA TX and RX channels will be configured so that it can transfer 4
    // bytes in a burst when the UART is ready to transfer more data.
    //
    ROM_UARTFIFOLevelSet(UART1_BASE, UART_FIFO_TX4_8, UART_FIFO_RX4_8);

    //
    // Enable the UART for operation, and enable the uDMA interface for both TX
    // and RX channels.
    //
    ROM_UARTEnable(UART1_BASE);
    ROM_UARTDMAEnable(UART1_BASE, UART_DMA_RX | UART_DMA_TX);

    //
    // This register write will set the UART to operate in loopback mode.  Any
    // data sent on the TX output will be received on the RX input.
    //
    HWREG(UART1_BASE + UART_O_CTL) |= UART_CTL_LBE;

    //
    // Put the attributes in a known state for the uDMA UART1RX channel.  These
    // should already be disabled by default.
    //
    ROM_uDMAChannelAttributeDisable(UDMA_CHANNEL_UART1RX,
                                    UDMA_ATTR_ALTSELECT | UDMA_ATTR_USEBURST |
                                    UDMA_ATTR_HIGH_PRIORITY |
                                    UDMA_ATTR_REQMASK);

    //
    // Configure the control parameters for the primary control structure for
    // the UART RX channel.  The primary contol structure is used for the "A"
    // part of the ping-pong receive.  The transfer data size is 8 bits, the
    // source address does not increment since it will be reading from a
    // register.  The destination address increment is byte 8-bit bytes.  The
    // arbitration size is set to 4 to match the RX FIFO trigger threshold.
    // The uDMA controller will use a 4 byte burst transfer if possible.  This
    // will be somewhat more effecient that single byte transfers.
    //
    ROM_uDMAChannelControlSet(UDMA_CHANNEL_UART1RX | UDMA_PRI_SELECT,
                              UDMA_SIZE_8 | UDMA_SRC_INC_NONE | UDMA_DST_INC_8 |
                              UDMA_ARB_4);

    //
    // Configure the control parameters for the alternate control structure for
    // the UART RX channel.  The alternate contol structure is used for the "B"
    // part of the ping-pong receive.  The configuration is identical to the
    // primary/A control structure.
    //
    ROM_uDMAChannelControlSet(UDMA_CHANNEL_UART1RX | UDMA_ALT_SELECT,
                              UDMA_SIZE_8 | UDMA_SRC_INC_NONE | UDMA_DST_INC_8 |
                              UDMA_ARB_4);

    //
    // Set up the transfer parameters for the UART RX primary control
    // structure.  The mode is set to ping-pong, the transfer source is the
    // UART data register, and the destination is the receive "A" buffer.  The
    // transfer size is set to match the size of the buffer.
    //
    ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART1RX | UDMA_PRI_SELECT,
                               UDMA_MODE_PINGPONG,
                               (void *)(UART1_BASE + UART_O_DR),
                               g_ui8RxBufA, sizeof(g_ui8RxBufA));

    //
    // Set up the transfer parameters for the UART RX alternate control
    // structure.  The mode is set to ping-pong, the transfer source is the
    // UART data register, and the destination is the receive "B" buffer.  The
    // transfer size is set to match the size of the buffer.
    //
    ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART1RX | UDMA_ALT_SELECT,
                               UDMA_MODE_PINGPONG,
                               (void *)(UART1_BASE + UART_O_DR),
                               g_ui8RxBufB, sizeof(g_ui8RxBufB));

    //
    // Put the attributes in a known state for the uDMA UART1TX channel.  These
    // should already be disabled by default.
    //
    ROM_uDMAChannelAttributeDisable(UDMA_CHANNEL_UART1TX,
                                    UDMA_ATTR_ALTSELECT |
                                    UDMA_ATTR_HIGH_PRIORITY |
                                    UDMA_ATTR_REQMASK);

    //
    // Set the USEBURST attribute for the uDMA UART TX channel.  This will
    // force the controller to always use a burst when transferring data from
    // the TX buffer to the UART.  This is somewhat more effecient bus usage
    // than the default which allows single or burst transfers.
    //
    ROM_uDMAChannelAttributeEnable(UDMA_CHANNEL_UART1TX, UDMA_ATTR_USEBURST);

    //
    // Configure the control parameters for the UART TX.  The uDMA UART TX
    // channel is used to transfer a block of data from a buffer to the UART.
    // The data size is 8 bits.  The source address increment is 8-bit bytes
    // since the data is coming from a buffer.  The destination increment is
    // none since the data is to be written to the UART data register.  The
    // arbitration size is set to 4, which matches the UART TX FIFO trigger
    // threshold.
    //
    ROM_uDMAChannelControlSet(UDMA_CHANNEL_UART1TX | UDMA_PRI_SELECT,
                              UDMA_SIZE_8 | UDMA_SRC_INC_8 |
                              UDMA_DST_INC_NONE |
                              UDMA_ARB_4);

    //
    // Set up the transfer parameters for the uDMA UART TX channel.  This will
    // configure the transfer source and destination and the transfer size.
    // Basic mode is used because the peripheral is making the uDMA transfer
    // request.  The source is the TX buffer and the destination is the UART
    // data register.
    //
    ROM_uDMAChannelTransferSet(UDMA_CHANNEL_UART1TX | UDMA_PRI_SELECT,
                               UDMA_MODE_BASIC, g_ui8TxBuf,
                               (void *)(UART1_BASE + UART_O_DR),
                               sizeof(g_ui8TxBuf));

    //
    // Now both the uDMA UART TX and RX channels are primed to start a
    // transfer.  As soon as the channels are enabled, the peripheral will
    // issue a transfer request and the data transfers will begin.
    //
    ROM_uDMAChannelEnable(UDMA_CHANNEL_UART1RX);
    ROM_uDMAChannelEnable(UDMA_CHANNEL_UART1TX);

    //
    // Enable the UART DMA TX/RX interrupts.
    //
    ROM_UARTIntEnable(UART1_BASE, UART_INT_DMATX | UART_INT_DMATX);

    //
    // Enable the UART peripheral interrupts.
    //
    ROM_IntEnable(INT_UART1);
}


//*****************************************************************************
//
// Initializes the uDMA software channel to perform a memory to memory uDMA
// transfer.
//
//*****************************************************************************
void
InitSWTransfer(void)
{
    uint_fast16_t ui16Idx;

    //
    // Fill the source memory buffer with a simple incrementing pattern.
    //
    for(ui16Idx = 0; ui16Idx < MEM_BUFFER_SIZE; ui16Idx++)
    {
        g_ui32SrcBuf[ui16Idx] = ui16Idx;
    }

    //
    // Enable interrupts from the uDMA software channel.
    //
    ROM_IntEnable(INT_UDMA);

    //
    // Put the attributes in a known state for the uDMA software channel.
    // These should already be disabled by default.
    //
    ROM_uDMAChannelAttributeDisable(UDMA_CHANNEL_SW,
                                    UDMA_ATTR_USEBURST | UDMA_ATTR_ALTSELECT |
                                    (UDMA_ATTR_HIGH_PRIORITY |
                                    UDMA_ATTR_REQMASK));

    //
    // Configure the control parameters for the SW channel.  The SW channel
    // will be used to transfer between two memory buffers, 32 bits at a time.
    // Therefore the data size is 32 bits, and the address increment is 32 bits
    // for both source and destination.  The arbitration size will be set to 8,
    // which causes the uDMA controller to rearbitrate after 8 items are
    // transferred.  This keeps this channel from hogging the uDMA controller
    // once the transfer is started, and allows other channels cycles if they
    // are higher priority.
    //
    ROM_uDMAChannelControlSet(UDMA_CHANNEL_SW | UDMA_PRI_SELECT,
                              UDMA_SIZE_32 | UDMA_SRC_INC_32 | UDMA_DST_INC_32 |
                              UDMA_ARB_8);

    //
    // Set up the transfer parameters for the software channel.  This will
    // configure the transfer buffers and the transfer size.  Auto mode must be
    // used for software transfers.
    //
    ROM_uDMAChannelTransferSet(UDMA_CHANNEL_SW | UDMA_PRI_SELECT,
                               UDMA_MODE_AUTO, g_ui32SrcBuf, g_ui32DstBuf,
                               MEM_BUFFER_SIZE);

    //
    // Now the software channel is primed to start a transfer.  The channel
    // must be enabled.  For software based transfers, a request must be
    // issued.  After this, the uDMA memory transfer begins.
    //
    ROM_uDMAChannelEnable(UDMA_CHANNEL_SW);
    ROM_uDMAChannelRequest(UDMA_CHANNEL_SW);
}

//*****************************************************************************
//
// Configure the UART and its pins.  This must be called before UARTprintf().
//
//*****************************************************************************
void
ConfigureUART(void)
{
    //
    // Enable the GPIO Peripheral used by the UART.
    //
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);

    //
    // Enable UART0
    //
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
    ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_UART0);

    //
    // Configure GPIO Pins for UART mode.
    //
    ROM_GPIOPinConfigure(GPIO_PA0_U0RX);
    ROM_GPIOPinConfigure(GPIO_PA1_U0TX);
    ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);

    //
    // Initialize the UART for console I/O.
    //
    UARTStdioConfig(0, 115200, g_ui32SysClock);
}

//*****************************************************************************
//
// This example demonstrates how to use the uDMA controller to transfer data
// between memory buffers and to and from a peripheral, in this case a UART.
// The uDMA controller is configured to repeatedly transfer a block of data
// from one memory buffer to another.  It is also set up to repeatedly copy a
// block of data from a buffer to the UART output.  The UART data is looped
// back so the same data is received, and the uDMA controlled is configured to
// continuously receive the UART data using ping-pong buffers.
//
// The processor is put to sleep when it is not doing anything, and this allows
// collection of CPU usage data to see how much CPU is being used while the
// data transfers are ongoing.
//
//*****************************************************************************
int
main(void)
{
    static uint32_t ui32PrevSeconds;
    static uint32_t ui32PrevXferCount;
    static uint32_t ui32PrevUARTCount = 0;
    uint32_t ui32XfersCompleted;
    uint32_t ui32BytesTransferred;

    //
    // Set the clocking to run directly from the crystal at 120MHz.
    //
    g_ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
                                             SYSCTL_OSC_MAIN |
                                             SYSCTL_USE_PLL |
                                             SYSCTL_CFG_VCO_480), 120000000);

    //
    // Enable peripherals to operate when CPU is in sleep.
    //
    ROM_SysCtlPeripheralClockGating(true);

    //
    // Enable the GPIO port that is used for the on-board LED.
    //
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION);

    //
    // Enable the GPIO pins for the LED (PN0).
    //
    ROM_GPIOPinTypeGPIOOutput(GPIO_PORTN_BASE, GPIO_PIN_0);

    //
    // Initialize the UART.
    //
    ConfigureUART();
	  UARTprintf("\033[2J\033[H");
    UARTprintf("uDMA Example\n");

    //
    // Show the clock frequency on the display.
    //
    UARTprintf("Tiva C Series @ %u MHz\n\n", g_ui32SysClock / 1000000);

    //
    // Show statistics headings.
    //
    UARTprintf("CPU\tRemaining\tMemory\t\t\t   UART\n");
    UARTprintf("Usage\tTime\t\tTransfers\t\t   Transfers\n");

    //
    // Configure SysTick to occur 100 times per second, to use as a time
    // reference.  Enable SysTick to generate interrupts.
    //
    ROM_SysTickPeriodSet(g_ui32SysClock / SYSTICKS_PER_SECOND);
    ROM_SysTickIntEnable();
    ROM_SysTickEnable();

    //
    // Initialize the CPU usage measurement routine.
    //
    CPUUsageInit(g_ui32SysClock, SYSTICKS_PER_SECOND, 2);

    //
    // Enable the uDMA controller at the system level.  Enable it to continue
    // to run while the processor is in sleep.
    //
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UDMA);
    ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_UDMA);

    //
    // Enable the uDMA controller error interrupt.  This interrupt will occur
    // if there is a bus error during a transfer.
    //
    ROM_IntEnable(INT_UDMAERR);

    //
    // Enable the uDMA controller.
    //
    ROM_uDMAEnable();

    //
    // Point at the control table to use for channel control structures.
    //
    ROM_uDMAControlBaseSet(pui8ControlTable);

    //
    // Initialize the uDMA memory to memory transfers.
    //
    InitSWTransfer();

    //
    // Initialize the uDMA UART transfers.
    //
    InitUART1Transfer();

    //
    // Remember the current SysTick seconds count.
    //
    ui32PrevSeconds = g_ui32Seconds;

    //
    // Remember the current count of memory buffer transfers.
    //
    ui32PrevXferCount = g_ui32MemXferCount;

    //
    // Loop until the button is pressed.  The processor is put to sleep
    // in this loop so that CPU utilization can be measured.
    //
    while(1)
    {
        //
        // Check to see if one second has elapsed.  If so, the make some
        // updates.
        //
        if(g_ui32Seconds != ui32PrevSeconds)
        {
					  //
            // Turn on the LED as a heartbeat
            //
            GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, GPIO_PIN_0);
					
            //
            // Print a message showing the CPU usage percent.
            // The fractional part of the percent value is ignored.
            //
            UARTprintf("%2u%%", g_ui32CPUUsage >> 16);

            //
            // Tell the user how many seconds we have to go before ending.
            //
            UARTprintf("\t%d seconds", 10 - g_ui32Seconds);
					
            //
            // Remember the new seconds count.
            //
            ui32PrevSeconds = g_ui32Seconds;

            //
            // Calculate how many memory transfers have occurred since the last
            // second.
            //
            ui32XfersCompleted = g_ui32MemXferCount - ui32PrevXferCount;

            //
            // Remember the new transfer count.
            //
            ui32PrevXferCount = g_ui32MemXferCount;

            //
            // Compute how many bytes were transferred in the memory transfer
            // since the last second.
            //
            ui32BytesTransferred = ui32XfersCompleted * MEM_BUFFER_SIZE * 4;
																 
						//
            // Print a message showing the transfer rate.
            //
            UARTprintf("\t%8u Bytes/Sec", ui32BytesTransferred);

            //
            // Calculate how many UART transfers have occurred since the last
            // second.  This expression is split to prevent a compiler warning
            // about undefined order of volatile accesses.
            //
            ui32XfersCompleted = g_ui32RxBufACount;
            ui32XfersCompleted += g_ui32RxBufBCount - ui32PrevUARTCount;

            //
            // Remember the new UART transfer count.  This expression is split
            // to prevent a compiler warning about undefined order of volatile
            // accesses.
            //
            ui32PrevUARTCount = g_ui32RxBufACount;
            ui32PrevUARTCount += g_ui32RxBufBCount;

            //
            // Compute how many bytes were transferred by the UART.  The number
            // of bytes received is multiplied by 2 so that the TX bytes
            // transferred are also accounted for.
            //
            ui32BytesTransferred = ui32XfersCompleted * UART_RXBUF_SIZE * 2;

            //
            // Print a message showing the transfer rate.
            //
            UARTprintf("\t%8u Bytes/Sec\n", ui32BytesTransferred);
						
						//
            // Turn off the LED.
            //
            GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, ~GPIO_PIN_0);
        }

        //
        // Put the processor to sleep if there is nothing to do.  This allows
        // the CPU usage routine to measure the number of free CPU cycles.
        // If the processor is sleeping a lot, it can be hard to connect to
        // the target with the debugger.
        //
        ROM_SysCtlSleep();

        //
        // See if we have run long enough and exit the loop if so.
        //
        if(g_ui32Seconds >= 10)
        {
            break;
        }
    }

    //
    // Indicate on the display that the example is stopped.
    //
    UARTprintf("\nStopped\n");

    //
    // Disable uDMA and UART interrupts now that the test is complete.
    //
    ROM_IntDisable(INT_UART1);
    ROM_IntDisable(INT_UDMA);

    //
    // Loop forever with the CPU not sleeping, so the debugger can connect.
    //
    while(1)
    {
			  //
        // Turn on the LED.
        //
        GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, GPIO_PIN_0);

        //
        // Delay for a bit.
        //
        SysCtlDelay(g_ui32SysClock / 20 / 3);

        //
        // Turn off the LED.
        //
        GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, 0);

        //
        // Delay for a bit.
        //
        SysCtlDelay(g_ui32SysClock / 20 / 3);
    }
}