Other Parts Discussed in Thread: HALCOGEN
Hi folks!
For first evaluations on the RM48 plattform I used the TMDSRM-USB-Kit. Currently I’m working with a Hercules RM48LM592PGE mounted on a custom board. During development I noticed some timing problems. An RTI configured to trigger after 1000us is fired after 22s. Same issues with the HET-Timers. A PWM-Signal with 50kHz leads to a measured clock of round about 2.3 kHz. There is a delay factor of ~22 !
I thought that reference clock is generated internally, but having a look on different schematics, it turned out that there is an external oscillator (Y1 16 Mhz). Well, this part is missing on our board. Is that the reason for the timing probs and where is the mcu getting the clock reference now? Because programming and debugging works fine….
And by the way: is there something like an assembly guide?!
Great forum guys. Keep it up!
Cheers
Jan