Other Parts Discussed in Thread: TM4C1294NCPDT
Hi.
I am trying to make a small SPI application with an Accelerometer unit. However, when I try to read the data out of it, I always see a value of 0xFF on the output through UART. I did set the CS line ( using Port B Pin 1) low before reading/writing data, and then high again when I'm done reading/writing data. I am using the exact code as in the TI/Peripheral/SSI/SPI-MASTER.
Please help me out as I have been stuck on this for the past 7 days. My code is as follows:
#include <stdint.h>
#include <stdbool.h>
#include <stdio.h>
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/gpio.h"
#include "drivers/pinout.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/rom_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "utils/uartstdio.h"
#include "driverlib/ssi.h"
#include "inc/tm4c1294ncpdt.h"
//===================================== INITIALIZE UART ON PORT A =================================================
//=================================================================================================================
void InitUART(void){
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
GPIOPinConfigure(GPIO_PA0_U0RX);
GPIOPinConfigure(GPIO_PA1_U0TX);
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);
GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
UARTStdioConfig(0, 115200, 16000000);}
//=================================================================================================================
//===================================== INITIALIZE SPI ON PORT D =================================================
//=================================================================================================================
void InitSSI(void){
ui32SysClock = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ | SYSCTL_OSC_MAIN | SYSCTL_USE_OSC), 25000000);
SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI2);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
SSIDisable(SSI2_BASE);
GPIOPinConfigure(GPIO_PD3_SSI2CLK);
GPIOPinConfigure(GPIO_PD2_SSI2FSS);
GPIOPinConfigure(GPIO_PD1_SSI2XDAT0);
GPIOPinConfigure(GPIO_PD0_SSI2XDAT1);
UARTprintf("\nTest Start");
GPIOPinTypeSSI(GPIO_PORTD_BASE, GPIO_PIN_3 | GPIO_PIN_2 | GPIO_PIN_1 | GPIO_PIN_0);
UARTprintf("\nTest Success");
SSIConfigSetExpClk(SSI2_BASE, ui32SysClock, SSI_FRF_MOTO_MODE_0,SSI_MODE_MASTER, 1000000, 8);
SSIEnable(SSI2_BASE);}
//=================================================================================================================
//===================================== NEW SPI WRITE FUNCTION ====================================================
//=================================================================================================================
void SSI2Write(uint32_t SSIData1,uint32_t SSIData2){
GPIO_PORTB_AHB_DATA_R &= ~(1<<1); // Make CS Line low
SysCtlDelay(24000000/3); // Slight Delay
while(SSIBusy(SSI2_BASE))
{}
SSIDataPut(SSI2_BASE, SSIData1);
SSIDataPut(SSI2_BASE, SSIData2);
while(SSIBusy(SSI2_BASE))
{}
SysCtlDelay(24000000/3); // Slight Delay
GPIO_PORTB_AHB_DATA_R |= (1<<1); //Make CS Line High
}
//=================================================================================================================
//===================================== NEW SPI READ FUNCTION ====================================================
//=================================================================================================================
uint32_t SSI2Read(uint32_t Addr, uint32_t Dummy){
uint32_t Data=0;
GPIO_PORTB_AHB_DATA_R &= ~(1<<1); // Make CS Line low
SysCtlDelay(240000/3); // Slight Delay
while(SSIBusy(SSI2_BASE))
{}
SSIDataPut(SSI2_BASE, Addr);
SSIDataPut(SSI2_BASE, Dummy);
while(SSIBusy(SSI2_BASE))
{}
SSIDataGet(SSI2_BASE,&Data);
while(SSIBusy(SSI2_BASE))
{}
SysCtlDelay(240000/3);// Slight Delay
GPIO_PORTB_AHB_DATA_R |= (1<<1); //Make CS Line High
return Data;
}
//=================================================================================================================
/=============================================== MAIN FUNCTION ====================================================
//=================================================================================================================
void main(void){
SysCtlClockSet(SYSCTL_SYSDIV_10 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);
SysCtlDelay(24000000/3); // INITIAL DELAY TO ALLOW ACCELEROMETER TO START UP IT'S REGISTERS
InitUART(); // SET UART ON PORT A
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
GPIO_PORTB_AHB_DEN_R |=(1<<1);
GPIO_PORTB_AHB_DIR_R |=(1<<1);
GPIO_PORTB_AHB_DATA_R |= (1<<1); // SETTING FOR PIN B1 TO BE CHIP SELECT LINE
InitSSI(); // SET SSI ON PORT D
UARTprintf("\nAddr: 0x18, Data: 0x38");SSI2Write(0x18,0x38);
UARTprintf("\nAddr: 0x10, Data: 0x60");SSI2Write(0x10,0x60);
UARTprintf("\nAddr: 0x0D, Data: 0x01");SSI2Write(0x0D,0x01); // START THE ACCELEROMETER
SysCtlDelay(24000000/3); //Slight Delay
while(1)
{uint32_t Data=SSI2Read(((0x22)|(0x80)),0x00);
UARTprintf("\nData Received: %i",Data);}
}
//=================================================================================================================